Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Accuracy of Real-Time Clock ION7650 / ION8650

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Accuracy of Real-Time Clock ION7650 / ION8650
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
570
Mehran_Mehrnia
Mehran_Mehrnia Champion
202
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
sesa243862_brid
sesa243862_brid Leader
Leader

Posted: ‎2016-10-11 01:44 PM

0 Likes
1
1142
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
‎2016-10-11 01:44 PM

Accuracy of Real-Time Clock ION7650 / ION8650

Hi.

Someone knows whats is the accuracy of the Real-Time Clock of ION7650 and ION8650?

I'm looking for this information.

Thanks in advance.

Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
sesa54412_bridg
sesa54412_bridg Contributor
Contributor

Posted: ‎2016-10-14 05:40 PM

0 Likes
0
1088
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
‎2016-10-14 05:40 PM

Hello Diego,

The accuracy of the real-time clock on the ION7650 and ION8650 meters depends on the the setting of the time synchronisation source:

If either meter is set to use its internal crystal for its time source, the meter's clock will drift up to ± 5 ppm and to a maximum of ± 10 ppm.

This means over the course of a day the meter's clock can drift from ~0.43 to 0.86 seconds. 

The actual clock drift will depend on the meter's installation temperature and how much that temperature varies over time.

If either meter is set to use a GPS time synchronisation protocol for its time source, the accuracy will be better than ± 1 msec, independent of the temperature.


In the GPS case, a meter's inputs can be used to accurately time-stamp events in Sequence of Events Recording (SER) applications:

Technical Library - Schneider Electric Schneider Electric


Please let us know if there are any other questions or if there are specific requirements for your application.


Kind Regards,

Chris Ailey

See Answer In Context

Reply
Reply 1
sesa54412_bridg
sesa54412_bridg Contributor
Contributor

Posted: ‎2016-10-14 05:40 PM

0 Likes
0
1089
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
‎2016-10-14 05:40 PM

Hello Diego,

The accuracy of the real-time clock on the ION7650 and ION8650 meters depends on the the setting of the time synchronisation source:

If either meter is set to use its internal crystal for its time source, the meter's clock will drift up to ± 5 ppm and to a maximum of ± 10 ppm.

This means over the course of a day the meter's clock can drift from ~0.43 to 0.86 seconds. 

The actual clock drift will depend on the meter's installation temperature and how much that temperature varies over time.

If either meter is set to use a GPS time synchronisation protocol for its time source, the accuracy will be better than ± 1 msec, independent of the temperature.


In the GPS case, a meter's inputs can be used to accurately time-stamp events in Sequence of Events Recording (SER) applications:

Technical Library - Schneider Electric Schneider Electric


Please let us know if there are any other questions or if there are specific requirements for your application.


Kind Regards,

Chris Ailey
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.