Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Invalid Links, Hosts and IP's in Netcon

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Invalid Links, Hosts and IP's in Netcon
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • Product_Support
    Product_Support
  • CraigEl
    CraigEl
  • Roger_Bently
    Roger_Bently
  • Cody_Failinger
    Cody_Failinger

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1933 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Invalid Links, Hosts and IP's in Netcon

Picard Product_Support
‎2018-09-07 01:51 AM

Last Updated: Administrator CraigEl Administrator ‎2022-08-09 01:21 AM

Issue

Invalid or phantom Links, Hosts and IP's in Netcon.  This symptom exists when you penetrate Network Configuration and there are Links and NPRs that you have no clue as to who they are or where they came from.

Product Line

TAC INET

Environment

  • I/NET
  • NPR-2000
  • Xenta 527

Cause

This can happen is if a laptop was used to connect to the system from a different Network or from the outside. Once connected, its IP address and any link it shares are broadcasted to the other devices like PCs and NPR’s, thus populating the table with entries that do not belong or are non-existent for this location or system. It can also happen if you install an NPR/527 or replace  one with a unit that has been used elsewhere. If that use NPR/527 is being used as a reference host, it will infect the system with every IP address and Link in its routing tables.

Resolution

At this point there is no way to get it out of the tables except to Telnet into all devices, remove the IP tables and rebuild them from scratch. This may be a cumbersome process depending on the amount of devices that make up the system (PCs, Laptops and NPR’s). All of these would need to be set back to 0 reference host while the cleanup is being done. To get this cleaned up, follow the steps to start a Telnet session:
 

  1. Go to Start > Run and type Telnet then hit Enter.
  2. Type open at the end of the prompt, hit the space bar and then put in the IP Address of the NPR/PC and hit Enter.
  3. A logon prompt will come up, type csi and hit enter
  4. Now type LA, this lists all the entries in the table.
  5. Type delall and hit enter. This clears out all the IP’s of the other devices.

This would have to be done on all the devices. Once completed, start I/NET to verify that those are gone and then start referencing other PC’s, Laptops and NPR’s to get the system back online again.

Note: The proper way to use a Service/Maintenance laptop that is used for multiple customer sites is to direct connect to the NPR to see the controllers of the other links that exist at the site. However, before starting I/NET on the service/maintenance PC, open Windows Explorer, C:\Program Files\Inet Seven and delete the XXX.dat files. These get rebuilt when I/O Server restarts, it also clears out all entries in the routing tables. See .DAT files. 
You may also create a different configuration profile for each site. This will also keep the tables separate.

Labels (1)
Labels:
  • TAC INET
Tags (1)
  • Find more articles tagged with:
  • 2168
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.