Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

BACnet device can't be discovered due to duplicate name

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • BACnet device can't be discovered due to duplicate name
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RobertAndriolo
    RobertAndriolo
  • CraigEl
    CraigEl
  • DavidFisher
    DavidFisher
  • Benji
    Benji
  • Cody_Failinger
    Cody_Failinger
  • AbeMeran
    AbeMeran
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
7798 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

BACnet device can't be discovered due to duplicate name

Picard Product_Support
‎2018-09-07 08:51 AM

Issue

BACnet device can't be discovered but instead shows up under the 'Unconfigured devices' in the server's hardware folder.

Product Line

EcoStruxure Building Operation

Environment

  • WorkStation
  • Enterprise Server - ES
  • Automation Server - AS

Cause

A BACnet device name must be unique. Devices with duplicate BACnet names can't be discovered.

In the screen shot below a device by the name AbesbCX already exists under Network1, when performing a device discovery on Network1 a second device with the same name is found, Since StruxureWare already has a device with the same name it adds the device to the list of unconfigurable devices.

NOTE:

“The <<N>> means the device was discovered on a directly connected network (such as the local IP network, or a directly connected MSTP bus).  The 2 indicates it was “port” 2, (port numbers are really an internal detail)

The server's Trace Log shows the following information, which includes the device's ID. The entry gives the reason as duplicate device name.

Resolution

1.8.1 and above

BACnet device name duplication is allowed, the duplicates will still land in the unconfigured folder and the system alarm will be generated BUT you can drag the duplicate device from the unconfigured folder to the desired network.

When finished, manually delete the device from the unconfigured/non-conformant folder. Alternatively, you can also  warm start the server to force the unconfigured/non-conformant devices list to be updated.

Note that the devices with duplicate names will still stay in the unconfigured/non-conformant folder until the name conflict is resolved.

1.7.2 and below

A workaround is to create the device manually and specify a BACnet name during the create process. When manually creating the device you need to know the Device ID, you can get the id from the information in the trace log as shown above.

SmartStruxure will send a message to the device to change its name to the specified BACnet name.

The entry in the unconfigured devices folder should automatically update after a few minutes, you can also re-start the server to force the unconfigured devices list to be updated, the entry for AbesBCX should be gone now that the devices has been manually configured.

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (5)
  • Find more articles tagged with:
  • 1.4.1.2009
  • 14717
  • CraigEllis20
  • defect23885
  • hotfix
Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.