This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2024-06-1106:34 AM
Connection bit in M580 PLC
How to get connection status from individual IO scanning connection in control expert. My PLC is M580. IO scanning is done from BMENOC0311.4. Which is placed in slot 3.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-07-2802:49 PM
I'm also curious about this. In Device DDT we can find a structure for the hardware used for IO scanning, in my case I use the CPU but it should look similar to the NOC I guess. In there we have DIO control and health bits which are called 513-640 and it say 1 BIT per DIO. These numbers corresponds nicely with the numbers in the DTM list which starts at 513. (lower numbers are used for RIO).
This may be the answer your question but then there is one more layer to it. In each device we can have several requests and each request also have it's own connection bit. At least for modbus TCP. Those bits are listed read only in the request row and also if you click on the device list in DTM browser list. These bits are called 1 and up. But how can we see/control these bits? Are they for health or control purposes or both?
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-07-2802:53 PM
Btw, I see now that this is posted completely wrong forum 😞 I stumbled upon it by searching and did not see that until now. Maybe a moderator can move it to Industrial Automation/PAC forum...