Support for vendor data from DNP3

Geo SCADA and Remote Operations Devices Ideas

Use this portal to submit your innovative ideas to make Geo SCADA Expert and Devices such as SCADAPack, Trio and Realflo of greater value to you and to the SCADA & Telemetry community. Every idea will be individually reviewed by our team for merit and will be marked Under Consideration.
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
  • Remote Operations
  • Geo SCADA and Remote Operations Devices Ideas
  • Support for vendor data from DNP3
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Labels
Top Labels
  • Alphabetical
  • SCADA 2
  • ViewX 2
  • Mimics 2
  • SCADAPack 2
  • Scripting 1
  • Virtual ViewX 1
  • Geo SCADA Expert 1
  • Efficiency 1
  • Configuration management 1
  • Modbus to WiStar 1
Idea Statuses
  • Submitted 13
  • Under consideration 126
  • Accepted 1
  • Declined 4
  • Partially delivered 0
  • Delivered 0
  • Abandoned 0
Related Products
Thumbnail of EcoStruxure™ Geo SCADA Expert
Schneider Electric
EcoStruxure™ Geo SCADA Expert
114
Thumbnail of SCADAPack 57x
Schneider Electric
SCADAPack 57x
2
Thumbnail of Accutech
Schneider Electric
Accutech
1
Load more
Completed Ideas
  • Accutech Modbus Master gateway to read Modbus devices and incorporate into WiStar net

  • Controller Key Enhancement

  • Restore "Embed Source Code for Upload" Option in Workbench (SP300 family)

  • DNP Outstation And DNP Master Diagnostics

View All
Top Liked Authors
User Likes Count
tfranklin
Commander tfranklin
15
aosburn
Lieutenant JG aosburn
8
ChrisHinton
Ensign ChrisHinton
1
gabarit
Lieutenant JG gabarit
1
View All

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
0 Likes

Support for vendor data from DNP3

Status: Under consideration Submitted by Spock BevanWeiss on ‎2021-10-11 12:24 PM
4 Comments (4 New)

With more DNP3 device vendors supporting Device Attributes, but the limitation of the Device Attribute options starting to show itself, it would be nice if some of the other DNP3 object types were supported within Geo SCADA Expert.

 

Additional support for the g0v211 "user-specific attributes" would be useful in this situation.

This would allow a vendor to insert additional information within the g0v211 data sets in accordance with the registered namespace, and for this to be displayed in Geo SCADA Expert (in the same way that Device Attributes are displayed).

 

I believe the configuration for this would be three entries on the Outstation Properties tabs (alongside the Device Attributes option).

The entries would be:

1. An enable / disable tick box

2. An option to specify when the user-specific attributes should be retrieved (a. Only Manually, b. On connection, c. On Integrity Poll.. or such)

3. A list of namespaces to retrieve, as comma separated values in a string i.e. "ABC Corp, XYZ Inc"

Tags (6)
  • Find more ideas tagged with:
  • english
  • scada
  • SCADA app
  • SCADA software
  • SCADA tutorial
  • Telemetry and SCADA
Comment

Link copied. Please paste this link to share this article on your social media post.

  • Back to Idea Exchange
  • Previous
  • Next
4 Comments
AndrewScott
Admiral AndrewScott
Admiral
‎2021-10-12 02:29 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2021-10-12 02:29 AM

All of the standard DNP3 device attributes, including the additional attributes added in DNP3 TB2013-004 (since 6.80) are supported.

The user-specific DNP3 device attributes (g0v211) are already supported (and have been since ~2009). This is key requirement for supporting the DNP3-WITS standard, which defines its own namespace.

All user-specific device attributes are automatically read whenever the device attributes are read. They are shown in the outstation's view status dialog.

When enabled, device attributes are automatically read whenever Geo SCADA starts comms with an outstation. Since, 6.80 there is also an option to only read device attributes following a master or outstation restart which can be more efficient.

There is also a 'Read Device Attributes' method (on the outstation) to trigger the attributes to be read on-demand.

BevanWeiss
Spock BevanWeiss
Spock
‎2021-10-12 07:13 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2021-10-12 07:13 AM

Thanks Andrew,

 

Is the Device Attribute request performed using a master request for g0 v254 qual=0?

Which then shows which user-specific attribute sets are advertised for a certain device.

Does it then enumerate through g0 v254 qual=xx for each user-specific attribute set index advertised?

 

Given the requirement to register an attribute-set with the DNP3 committee.. this may not be the best mechanism for the vendor to expose custom device attribute data via DNP3.  I'm open to other ideas on this.

The issue is becoming that certain vendors that we work with are starting to present this data in ways that make it 'awkward' to handle reliably and securely within Geo SCADA Expert (i.e. exposing it as a INF format file, hence suggesting the use of DNP3 File Transfer to retrieve and then parse for information).

AndrewScott
Admiral AndrewScott
Admiral
‎2021-10-12 10:40 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2021-10-12 10:40 AM

Is the Device Attribute request performed using a master request for g0 v254 qual=0?

Which then shows which user-specific attribute sets are advertised for a certain device.

Does it then enumerate through g0 v254 qual=xx for each user-specific attribute set index advertised?

Yes, this is defined by the DNP3 standard.

 

I don't think the 'requirement' to register namespaces with the DNP3 committee is very important as long as the chosen name is unique, e.g. it includes the vendor's name. Most vendors haven't bothered registering their namespaces:

https://www.dnp.org/Resources/DNP-Namespaces 

 

Non-standard solutions using proprietary file formats are never going to deliver interoperability. Geo SCADA could read the file and save it to disk but that's all without developing a custom DNP3 driver extension that can parse the custom file format and store the resulting attributes.

sbeadle
Kirk sbeadle Kirk
Kirk
‎2022-08-02 05:39 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2022-08-02 05:39 AM
Status changed to: Under consideration

Thank you.

Comment
Preview Exit Preview

never-displayed

Hint:
@ links to members, content
 
  • Back to Idea Exchange
  • Previous
  • Next
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.