Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

ClearSCADA 2015 R2 Operating System Support

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • ClearSCADA 2015 R2 Operating System Support
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Python API - Reading the Instance and Template Structure
  • Python API - How to get Earthquake data into a Geo SCADA Map
  • Python API - Creating and Configuring Data Tables
  • Python API - Setting aggregates
  • Python API - Clearing an aggregate link
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Anonymous user
Not applicable
‎2021-06-09 01:43 PM
0 Likes
0
955
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
‎2021-06-09 01:43 PM

ClearSCADA 2015 R2 Operating System Support

Originally published on Geo SCADA Knowledge Base by Anonymous user | June 09, 2021 10:43 PM

📖 Home  Back  
Systems running on server hardware need to use server operating systems such as Windows Server 2012 or Windows Server 2008 R2. Server operating systems are designed for servicing entire systems rather than individual computers or small networks and so are better suited for larger SCADA Expert ClearSCADA systems with more than two clients.

Systems running on desktop hardware should run desktop operating systems such as Windows 8 or Windows 7. Desktop operating systems are designed for user interaction on the computer on which they are installed.

Desktop operating systems should not be used for servers with more than two clients as the TCP/IP security measures in these operating systems can cause significant delays.

Refer to the following table for supported Operating System versions:
    32-Bit   64-Bit
  Desktop Hardware   Windows 10 (Professional and Enterprise editions)
Windows 8.1 (Professional and Enterprise editions)
Windows 8 (Professional and Enterprise editions)
Windows 7 (Professional and Ultimate editions) - Service Pack 1
  Windows 10 (Professional and Enterprise editions)
Windows 8.1 (Professional and Enterprise editions)
Windows 8 (Professional and Enterprise editions)
Windows 7 (Professional and Ultimate editions) - Service Pack 1
  Server Hardware   Nil   Windows Server 2012 R2 (Standard and Datacenter editions)
Windows Server 2012 (Standard and Datacenter editions)
Windows Server 2008 R2 (Standard and Enterprise editions) - Service Pack 1


SCADA Expert ClearSCADA also requires Internet Explorer 9 (32-bit), 10 (32 bit) or 11 (32-bit) for both software installation and fully-functional web-based operation. The new WebX User Interface available from ClearSCADA 2015 R1 is accessible from any HTML5 browser for viewing of Trends, Alarm Lists, Event Lists, and Queries from various types of phone, tablet or laptop.
Web and Mobile Server: The Web server available in ClearSCADA 2015 R2 is 64-bit only and therefore not available to install on 32-bit computers. This feature must be installed on the server(s) to use the new WebX User Interface.




The original integrated WebX is still available for both 32-bit and 64-bit computers.

Known Issues: Please refer to the Known Issues for more details about compatibility issues between ClearSCADA 2015 R2 and Internet Explorer 9/10/11.

Legacy Operating Systems: ClearSCADA 2015 R2 does not include support for Windows XP, Windows Server 2003, Windows Vista or Windows Server 2008 R1.


Go: Home Back

Author

Biography

Anonymous user

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.