Posted: 2017-05-22 10:32 AM
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
Please link demo for COM'X 210
Hi exxperts,
I want research and configuration COMX_210. But, now i don't product.
You can give me DEMO LINK access COMX_210 just like demo link for EGX 150.
Thanks very much
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
**Sneak Peek** Com'X 510 Demo Available online... If you can configure a 510 then a 200 should be even easier Maybe James Jeanette can confirm if these are still the correct credentials.

Posted: 2017-05-23 08:56 AM
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
HI Letagan,
Thanks for your insformation. But i can't access. Error snapshot display below. Can you help me?
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
Select "Continue..."
You may have to request or verify the password. I'm not sure if the credentials are still valid.

Posted: 2017-05-25 10:58 PM
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
Hi Lategan,
Thanks very much. I have to access.
But not least. Address IP default of COM'X 210?
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
Our units had DHCP so a connected router will provide an IP. Use Windows Network device search to find Com'X device to get access. We are using one in our lab in Menasha Wisconsin USA to display and push data to Schneider Facility Insights Cloud software. Our Com'X is a 510. These do not natively support some legacy devices, however you can create custom devices that work OK. Here is a screen-shot of some of our meters.