Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
EcoStruxure Panel Server Edge 1.2 & EcoStruxure Power Commission-Desktop 2.22.1 RELEASED
Edge 1.2 Firmware and EPC Desktop 2.22.1 are now available on se.com.
Discover the new features delivered with Edge 1.2 Release. Explore the updated User Guide and Cybersecurity Guide
Access all Panel Server assets on Exchange Extranet.
Link copied. Please paste this link to share this article on your social media post.
Thanks @Romain_Polette The software didn't work with a factory default reset PAS600L connected to a W10 laptop with latest Windows Patches (related screenshots and log file attached), but worked on another W10 computer. this didn't happen when creating a project.
Link copied. Please paste this link to share this article on your social media post.
If a link to the latest firmware RAUCB file could be posted for installation using the webserver, that would be appreciated.
(The SEDP file doesn't seem to be the file type needed for firmware update over webserver)
Link copied. Please paste this link to share this article on your social media post.
Hi @swil ,
I cannot help with your EPC 2.22.1 issue. I found some unexpected messages in the EPC Logs like :
Regarding your PAS600:
Thanks.
Regardsi,
Link copied. Please paste this link to share this article on your social media post.
It's assumed the PAS600Ls are production units. The log zip file attachment is provided in a post above (likely from a device with FW 1.1.1)
EPC did not allow creation of Switchboards with PAS600Ls with FW 001.001.001 (on my laptop with SQL installed), and with FW 001.002.001 on a colleague's laptop (unsure if SQL installed on that).
EPC worked on another laptop without SQL server installed for FW 1.1.1 and FW 1.2.1.
Link copied. Please paste this link to share this article on your social media post.
Dans une futur version, ce bien de faire une modification.
Lorsque l'on a plusieurs départs ou arrivées équipés de TH110, le Panel Server peut être en alarme (clignotement orange).
Pour nous ce n'est pas forcement une alarme, certaines arrivées ou certains départs peuvent être volontairement hors tension.
Ce clignotement peut perturber le client qui va penser qu'il y a un problème.
In a future version, it's good to make a change.
When there are several feeders or incomers equipped with TH110, the Panel Server may be in alarm (flashing orange).
For us it is not necessarily an alarm, some arrivals or some departures may be voluntarily off.
This flashing can disturb the customer who will think that there is a problem.
#panelserver
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.