Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Does EGX300 supports to read on-board log in PM800?

Gateways and Energy Servers

Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
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
  • EcoStruxure Power & Grid
  • Gateways and Energy Servers
  • Does EGX300 supports to read on-board log in PM800?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Romain_Polette
Kirk Romain_Polette Kirk
117
Guillaume_Evrard
Captain Guillaume_Evrard Captain
59
Randi_Dolan
Commander Randi_Dolan Commander
46
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Gateways and Energy Servers
Start a Topic
Solved
QuanGUO
Lieutenant QuanGUO Lieutenant
Lieutenant

Posted: ‎2013-05-29 06:17 PM

0 Likes
3
946
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
‎2013-05-29 06:17 PM

Does EGX300 supports to read on-board log in PM800?

We are discussing if EGX300 can retrieve the on-board log in PM800 in case the communication is failure, and saving these data as Datalog in EGX300?

1676

Tags (1)
  • Tags:
  • datalog
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
sesa82384_bridg
sesa82384_bridg Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2013-05-30 02:16 AM

0 Likes
2
874
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
‎2013-05-30 02:16 AM

Hello Quan, no, it can't do that. You are totally right in the hardware architecture. But there is no such software functionality to make it happen.

This is not a feature in EGX or any other gateway we have in Schneider at global offer.

This is also true for the high end meters like CM4000 and ION.

See Answer In Context

Reply
Replies 3
sesa82384_bridg
sesa82384_bridg Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2013-05-30 02:16 AM

0 Likes
2
875
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
‎2013-05-30 02:16 AM

Hello Quan, no, it can't do that. You are totally right in the hardware architecture. But there is no such software functionality to make it happen.

This is not a feature in EGX or any other gateway we have in Schneider at global offer.

This is also true for the high end meters like CM4000 and ION.

Reply
QuanGUO
Lieutenant QuanGUO Lieutenant
Lieutenant

Posted: ‎2013-05-30 02:24 AM

0 Likes
0
874
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
‎2013-05-30 02:24 AM

Thanks for this clarification Carlos.

Reply
sesa64390_bridg
Lt. Commander sesa64390_bridg Lt. Commander
Lt. Commander

Posted: ‎2013-06-03 09:55 AM

0 Likes
0
874
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
‎2013-06-03 09:55 AM

just in addition the reason this doesn't work this way is because the EGX300 essentially acts as a modbus master and just polls the downstream devices (PM800 in this case) for the readings (as exposed via the PM800 holding registers) when triggered by the 'Interval Reading' setting you set in the EGX300 (ie 10, 15, 30 mins or 1hr reading intervals). So in the case you have above the EGX300 (if powered at the time) would register an ERROR in the data file when the data file is created.

The EGX300 only creates a dat file in .csv format when the logging is enabled on the EGX300 and there are readings saved in the binaries.

EODC when it reads the ERROR (25 or 38 usually - but please see the EGX300 User Guide for the full list of errors) will simply skip that channel.datapoint. If you have the EODC task: Data Quality: Interval Gap Filler enabled then EODC will fill in missing intervals via linear interpolation if the gap is within the file (and there are valid measurements after the gap in the same data file ie used for when 1 or 2 measurements are missing).

Usually the kind of interruption you describe is due to a power outage on the EGX300 (because if it was an outage on the PM800 then line voltage is usually down too and therefore no energy is measured). In this case we always recommend UPS supplies on the EGX300.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.