Communications problems with a EGX100
Hello everyone.
I have a customer that he has a EGX100 and in the MODBUS there are about 20 power meters. He has PM710, PM5560 and ION6200.
He has the EGX100 connected to a EGX300, and he can see all power meters registers, except the ION6200.
The MODBUS was checked and its OK. Electrical conections are fine.
Wich can be the problem, any have any idea?
Thanks for all.
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
Hello,
I am not 100% what you mean by "The MODBUS was checked and its OK." if this checking the wires or the modbus settings on the ION 6200 meter. The ION 6200 Meter has a setup register that determines what protocol the meter talks. either PML or Modbus. Will want to check that the meter is set to talk modbus.
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
Thanks, I will check it!
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
Hi Carlos,
What did you find?
Grant
![](/skins/images/D7B476B56A4C92CBBF0CFB88116B0F92/responsive_peak/images/icon_anonymous_message.png)
![](/skins/images/D7B476B56A4C92CBBF0CFB88116B0F92/responsive_peak/images/icon_anonymous_message.png)