Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Posted: 2017-08-25 06:54 AM
Link copied. Please paste this link to share this article on your social media post.
Hi Hastak,
Sorry to hear that happened to your ComX510. I think at this point most likely the ComX is permanently damaged, but you may try PoE (power over ethernet) to see if the ComX will come online.
Best Regards,
Colton
Posted: 2017-08-25 06:54 AM
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Colton Peltier - Yes you are right!! After your message I tried connecting on POE and it booted up and I can log in.
Unfortunately the site that I am working with, doesn't have POE, but I can reuse the Com'X box in demo in our office in SG.
Thanks for the comment and hint. Very helpful!!
Yeh Wei LOH and Kuan Khoon TAN - FYI
Link copied. Please paste this link to share this article on your social media post.
Good to know that PoE still works as it feeds the internal circuity via another path not affected by the 24V DC-DC convertor. Unfortunately, it is not an "alternative" or "recovery"solution as 230/240Vac should have never been fed into the ComX 510 in the first place. It is extremely hazardous and it may result in fires and extensive property damage.
My take is that the connector on the SmartLink Si D should be re-designed to make sure it cannot fit the 24Vdc connections that is prevalent in our low voltage offers (i.e. IF-E, ComX, Link150, FDM121, Magelis, etc.). Granted the connector can take 240Vac, it makes absolutely no sense for a 240Vac connection to use the same connector/removable plug as a 24Vdc connection within the same manufacturer (worse still, within the same offer umbrella).
My 2 cents worth.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.