Posted: 2020-07-05 01:32 PM . Last Modified: 2024-04-04 12:29 AM
how to configure netbotz 150 to netbotz 250
Hello, how to thread netbotz 150 to netbotz 250
The netbotz 150 does not turn on and is connected to 250?
thanks
(CID:134690872)
- Labels:
-
NetBotz
Link copied. Please paste this link to share this article on your social media post.
Accepted Solutions
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
Posted: 2020-07-05 01:32 PM . Last Modified: 2024-04-04 12:29 AM
Hi Roni,
If you have the NetBotz 250 up and running, all you should need to do is to connect the 150 to the A-link port on the 250 using a cat-% cable (some issues have been seen with cat-6 but it should still power on).
Please make sure the 250 is up to date on it's firmware.
Make sure the 250 can see it's own internal sensor pod and there are no errors.
Thanks,
Steve
(CID:134690885)
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
Posted: 2020-07-05 01:32 PM . Last Modified: 2024-04-04 12:29 AM
Hi Roni,
If you have the NetBotz 250 up and running, all you should need to do is to connect the 150 to the A-link port on the 250 using a cat-% cable (some issues have been seen with cat-6 but it should still power on).
Please make sure the 250 is up to date on it's firmware.
Make sure the 250 can see it's own internal sensor pod and there are no errors.
Thanks,
Steve
(CID:134690885)
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
Posted: 2020-07-05 01:32 PM . Last Modified: 2024-04-04 12:29 AM
Hi.
I need to connect to the network or to the sensor?
(CID:134690904)
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
Posted: 2020-07-05 01:32 PM . Last Modified: 2024-04-04 12:28 AM
Hi roni,
The sensor pod 150 does not connect to your network. You do use a network type cable but the a-link ports on the 250 are meant only for the sensor pod 150 or other a-link sensors.
Here's the example from the NetBotz 250 manual:
Which can be found here:
https://www.schneider-electric.us/en/download/document/APC_JLER-A4CL7S_EN/
Thanks,
Steve
(CID:134690914)
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
Posted: 2020-07-05 01:32 PM . Last Modified: 2023-10-22 04:37 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.