Posted: 2020-07-04 08:36 PM . Last Modified: 2024-04-04 04:08 AM
Why are DCO reports semi-colon delimited rather than comma and essentially impossible to organize?
I get that "CSV" is being used as a generic term.
But we really need to be able to parse this file so it can be usefully sorted.
The file is semi-colon delimited, yet the information is not broken down enough to be well organized or sorted.
Example - inventory file
the Name, Location, Barcode, Part Number, and Description columns are semi-colon delimited.
However, the details of the location are separated by a "/"
And then there are some "," between elements of the details about the Item Description for products from APC - so irrelevant
Any person managing a facility needs to be able to sort by :
Row
Rack
Rack Unit
Having all of those in 1 cell, makes it hard to work with -
You also have the "left-rear" and such that need to be isolated from other location information -
These inventory reports and export files need to be delimited to a greater degree and by a single delimiter.
When can this change be implemented ?
(CID:132667802)
- Labels:
-
Data Center Operation
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
Posted: 2020-07-04 08:36 PM . Last Modified: 2024-04-04 04:08 AM
Hello Eric
This change was made to DCO a while back because there are field elements which contain comma's so it was causing problems for some customers.
However, under the tools-preferences menu option, expand the general pane and select 'csv export', you can select comma or semicolon as the delimiter used in in DCO exports. I pasted a screenshot below for reference purposes.
Regards
GregS
(CID:133370387)
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
Posted: 2020-07-04 08:36 PM . Last Modified: 2024-04-04 04:08 AM
To add to Greg's comment:
Perhaps exporting out from Equipment browser better fits your need?
You can select to show the following columns to supplement location:
Room
Row
Rack
U space
Refer to Christian Riis' tips on using equipment browser:
Regards,
Chris
(CID:133370390)
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
Posted: 2020-07-04 08:36 PM . Last Modified: 2023-10-22 04:21 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.