EcoStruxure IT forum
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 10:49 PM . Last Modified: 2024-04-04 02:45 AM
I 'am using DCE 7.2. Can I upgrade ecostrucureit ? how to to ? kindly help.
and I would like to recieve Alarm via audio when I have warning alarm.
(CID:134027117)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 10:49 PM . Last Modified: 2024-04-04 02:45 AM
Hi Nguyen,
If you want to use your DCE to connect to EcoStruxure IT, then you would initially need to upgrade your DCE to the latest version (currently DCE 7.5). Upgrading the product to latest version by the way is usually a good practice and highly recommended. And then read the following guide: https://struxureon.com/connect-from-data-center-expert/
However, EcoStruxure IT Gateway can be setup independent of DCE, for more details please see the following guide: https://struxureon.com/download-and-set-up-struxureon-gateway/
Additional/related info here: Getting started with EcoStruxure IT
Concerning the Alarm via audio, additional to the device (smart phone) sound settings, notifications and sound settings can be configured from the App: Settings > Notifications
Kind regards
(CID:134027158)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 10:49 PM . Last Modified: 2024-04-04 02:45 AM
Dear Nguyen Quoc Son,
In short, everything depends on what you want to get for yourself as a result. At the moment there are officially two digital services Schneider Electric.
To connect to the first digital service EcoStruxure IT Expert, you need to use a separate free EcoStruxure IT Gateway software (your DCE server is not used here) connected to the cloud Schneider Electric servers. After paying for a subscription to a digital service, you will have a web-GUI based monitoring system via Internet with an overview of existing alerts and statistics on devices and their sensors. In addition, you will have a mobile application (for Android or iOS) with similar functionality and capabilities (for example, real time alert and incident notification).
To connect to the second digital service EcoStruxure Asset Advisor you need your DCE-server, but updated to the latest version 7.5.0 – is important. This DCE-server also needs to be connected to the cloud servers of Schneider Electric. After paying for a subscription to a digital service, you will have, in addition to your standard DCE interface and alerting system, a monitoring system based on a web-GUI interface over the Internet, reviewing existing warnings/alerts and statistics on devices and their sensors. In addition, you will have a mobile application (for Android or iOS) with similar features and capabilities (for example, real time alert and incident notification). This digital service is more advanced, allows the end customer to perform parallel migration, but also costs more.
More details about the differences between these two digital services are written in the recent topic .
I hope this helps you.
With respect.
(CID:134027164)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 10:49 PM . Last Modified: 2024-04-04 02:45 AM
Dear Nguyen Quoc Son,
Tell us, please, did you solve your question or not?
With respect.
(CID:134680052)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 10:49 PM . Last Modified: 2023-10-22 04:04 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.