EcoStruxure IT forum
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 10:16 AM . Last Modified: 2024-04-10 12:57 AM
With the upgrade to 7.4.5 there is now a serial number field on the General tab for a device. However we have the serial number field in the Properties (Custom) tab which also includes a unique and mandatory check on it.
(CID:93914397)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 10:16 AM . Last Modified: 2024-04-10 12:57 AM
Hi James, we will look into it, thanks for posting.
(CID:93914434)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 10:16 AM . Last Modified: 2024-04-10 12:57 AM
Hi James,
There has been no additional features applied to the serial number field.
It is possible to capture a serial number in the new introduced field. There are no way to move existing serial numbers in custom properties into the new field automatically. Currently it must be a manual process. Also the field has no check on if it is unique or mandatory.
I will track the feature of moving an existing custom property into the serial number property field as a feature request.
In regards to unique-ness I guess that is not always what you want? I guess the serial number might be the same from different vendors? Also the mandatory field could you elaborate a bit on that, since I guess you would only like it to be mandatory on some type of equipment?
(CID:93914457)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 10:16 AM . Last Modified: 2024-04-10 12:56 AM
Soren,
For the serial number field we have a unique check on it to try and eliminate any errors. I have never seen a serial number the same on two different devices from two different manufacturers so its not a problem that has occurred (not saying it might not happen). It would be good to have the option to turn it on or off as per the Configure Custom Properties tab.
The other problem we have now is there are three Serial Number fields,
We had to add the Custom Properties one due to the lack of the field in the program originally.
(CID:93914529)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 10:17 AM . Last Modified: 2024-04-10 12:56 AM
Hi James, Thank you for elaborating this is valuable input. I will track all your comments in the request. It is not possible for me to tell when this will make it into the program but it will be tracked and thereby also very likely find its way in a future release.
(CID:93914531)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 10:17 AM . Last Modified: 2023-10-31 11:34 PM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.