EcoStruxure IT forum
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-05 05:46 PM . Last Modified: β2024-04-03 03:15 AM
Hi,
We have two Netbotz 570 connected to DCE and after setting the NTP sources on them we started receiving notifications "Critical Communication error with device IP - The device is offline due to a timeout or connection error." from DCE.
After that we are also unable to connect to the Netbotz devices with Advanced View.
How can I regain access to the devices and remove the NTP server from the configuration?
Thanks in advance.
Rodrigo Catarino
(CID:140711663)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-05 05:46 PM . Last Modified: β2024-04-03 03:14 AM
Hi Rodrigo,
If you reboot the appliance, are you still unable to access it?
Do you know what version of firmware is on the appliance?
Is the only recent change the NTP server? I've not heard of this being an issue. If it's a public NTP, I'd like to test it too.
DCE and AV use the same HTTP / HTTPS protocols to communicate to the appliance. I'm assuming you can not browse to the appliance either. I would first suggest you verify serially that the IP of the appliance has not changed. If not, then about the only thing left is to reset the appliance to defaults. K-base FA158175 explains how this can be done.
Steve.
(CID:140711760)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-05 05:46 PM . Last Modified: β2024-04-03 03:14 AM
Hi Rodrigo,
If you reboot the appliance, are you still unable to access it?
Do you know what version of firmware is on the appliance?
Is the only recent change the NTP server? I've not heard of this being an issue. If it's a public NTP, I'd like to test it too.
DCE and AV use the same HTTP / HTTPS protocols to communicate to the appliance. I'm assuming you can not browse to the appliance either. I would first suggest you verify serially that the IP of the appliance has not changed. If not, then about the only thing left is to reset the appliance to defaults. K-base FA158175 explains how this can be done.
Steve.
(CID:140711760)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-05 05:46 PM . Last Modified: β2024-04-03 03:14 AM
Hi Steve,
Yes, i've rebooted the appliance and still unable to access it.
The appliance firmware version is 4.6.2 (Build: 20171031_1416)
I am no able to connect to it either via web, telnet or advanced view.
is it possible to perform a backup of the configuration via serial port?
Thanks in advance.
Rodrigo
(CID:140711856)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-05 05:46 PM . Last Modified: β2024-04-03 03:14 AM
Hi Rodrigo,
Sorry, no. You must have http or https access to the appliance in order to create a backup. Additionally, if there is a configuration issue that is causing this, re-importing a backup with this bad configuration would likely cause the same issue again as you can not edit a backup.
Steve
(CID:140711859)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-05 05:46 PM . Last Modified: β2023-10-22 03:20 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.