Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84695members
354074posts

DCE TCP Modbus output with two network interfaces

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

Solved
jzurera
Lieutenant
Lieutenant
0 Likes
1
250

DCE TCP Modbus output with two network interfaces

Hi,

 

we have a DCE 7.9 with Modbus Output licence and we have a doubt, this DCE has two network interfaces, a public lan and a private lan with all the monitored devices. 

 

Is the output modbus available in both network interfaces?

 

Thanks in advance

Tags (1)

Accepted Solutions
Shaun
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
246

Re: DCE TCP Modbus output with two network interfaces

Hi @jzurera,

 

The modbus output does listen on all interfaces when enabled.  It doesn't listen unless licensed. 

See Answer In Context

Tags (1)
1 Reply 1
Shaun
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
247

Re: DCE TCP Modbus output with two network interfaces

Hi @jzurera,

 

The modbus output does listen on all interfaces when enabled.  It doesn't listen unless licensed. 

Tags (1)