Posted: 2020-07-02 09:13 AM . Last Modified: 2024-04-10 01:17 AM
DCE 7.2.4.42 VM is sluggish
We have purchased a virtual appliance license and are planning on migrating from the physical box. The virtual client is considerably slower than the physical unit. The desktop client takes approximately 2-2:30 minutes with no devices configured to connect to the vm. Our physical box with all of our devices configured and monitored takes approximately 6 seconds.
I am reluctant to continue with the migration with this kind of delay. The ESX host and the physical DCE box are in the same location and network throughput looks good. CPU utilization never goes over 6% according to the VM stats.
Current VM build Specs:
VM Version: 7
CPU: 4 vCPU
Memory: 4096 MB
Memory Overhead: 64.86 MB
VMware Tools: Running
Consumed Host CPU: 63 MHz
Consumed Host Memory: 1697 MB
Active Guest Memory: 163 MB
Provisioned Storage: 272 GB
Is anyone else having this problem?
(CID:93192473)
- Labels:
-
Data Center Expert
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
Posted: 2020-07-02 09:14 AM . Last Modified: 2024-04-10 01:17 AM
(CID:93192731)
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
Posted: 2020-07-02 09:14 AM . Last Modified: 2024-04-10 01:17 AM
Hi Christopher, Have you looked through this thread with somewhat the same issue as you are experiencing? The thread also has a number of questions asked by Breda which is the next step to understand why this issue is occurring.
(CID:93192807)
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
Posted: 2020-07-02 09:14 AM . Last Modified: 2024-04-10 01:17 AM
I am having the same issue. The VM takes forever to find devices, create new folders, etc. I ran a device search several times for the same IP and it took maybe 5 minutes to actually show up in the unassigned folder.
I too was going to migrate over from the appliance however with this latency issue, that isnt going to happen until it is fixed.
The VM itself seems to be running fine. Although memory is up to 80% usage. I am using the maximum 4GB of RAM and per the specs it can't use anymore.
My VM is almost maxed out on storage at around 300GB. I am working to increase this to 500GB however I doubt that will fix this issue since it has been going on for awhile now.
Regards,
J
(CID:93193864)
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
Posted: 2020-07-02 09:14 AM . Last Modified: 2023-10-31 10:24 PM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.