Posted: 2020-07-03 09:34 AM . Last Modified: 2024-04-08 03:30 AM
Connecting devices with NO/NC dry contact to DCE AP9465 Server
Hi,
In one of our projects, client wants to connect below devices with NO/NC dry contacts to DCE AP9465 Server:
- Fuel Tank
- Generator 1
- Generator 2
- Main Gate DSM "Door status monitor"
I understand that we have modbus rs485 to tcp/ip converter (TSXETG100) but for the above can anyone suggest a device.. may be a third party device which was tested and working?
Thanks & Regards
Shemil
(CID:110012070)
- Labels:
-
Data Center Expert
Link copied. Please paste this link to share this article on your social media post.
Accepted Solutions
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
Posted: 2020-07-03 09:34 AM . Last Modified: 2024-04-08 03:30 AM
Hi Shemil, you can also use the Netbotz 250 (NBRK0250) in combination with the dry contact cables, connected to the Universal sensor ports
Used for connecting APC sensors and third-party dry contact sensors. (See “Connect
sensors to universal sensor ports” on page 12 for a list of applicable APC sensors.) Thirdparty
dry contact sensors require a NetBotz Dry Contact Cable (NBES0304).
This Netbotz can be connected to you're generator via the dry contact cables and the netbotz itself can then be monitored via the DCE
(CID:110012130)
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
Posted: 2020-07-03 09:34 AM . Last Modified: 2024-04-08 03:30 AM
Hi Shemil,
You can easily use Schneider Automation Server for such requirements which can again hook back to SXW DCE. See my post here:
(CID:110012075)
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
Posted: 2020-07-03 09:34 AM . Last Modified: 2024-04-08 03:30 AM
Hi Shemil, you can also use the Netbotz 250 (NBRK0250) in combination with the dry contact cables, connected to the Universal sensor ports
Used for connecting APC sensors and third-party dry contact sensors. (See “Connect
sensors to universal sensor ports” on page 12 for a list of applicable APC sensors.) Thirdparty
dry contact sensors require a NetBotz Dry Contact Cable (NBES0304).
This Netbotz can be connected to you're generator via the dry contact cables and the netbotz itself can then be monitored via the DCE
(CID:110012130)
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
Posted: 2020-07-03 09:34 AM . Last Modified: 2023-10-20 05:10 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.