EcoStruxure IT forum
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-10-28 08:18 AM
Hello,
I have a problem with the APC NetBotz 750.
Im connected directly to the NetBotz via lan cable. The connection to the gui is really bad and it disconnects every fifth ping. When I change the settings of the adapter from 1 GIG to 100 GIG it works perfectly fine and the ping doesnt break up. Its the same with direct connect and even with another notebook. Is 1 GIG not supported?
Another problem is that the NezBotz disconnects the camera sensor which is connected via wlan.
All of the sensores are keep getting lost over the day and need to be new discovered.
The newest firmware is already installed (V. 5.4).
Can someone explain please?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-10-29 07:51 AM
Hello @NMMS,
I would recommend reaching out to technical support on this matter. They likely will gather some advanced log files and see if there is anything going on with the NetBotz appliance that is affecting your sensors. You can also discuss with them your issues with using a 1GB network connection.
Kind Regards,
Cory
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-12-05 01:33 PM
I'm seeing the same issues. configure switchport to 100mb/full, and no issues, but 1gb has issues with ping and connectivity.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.