Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-09-30 01:26 AM
I have setup a new NetBotz 750 system, a few sensor POD is showing device ID 88.
I have seen this number when the system is starting up, or when it updates the firmware.
The NetBotz is showing the following alarms:
I have noticed that I have to sensor pod with ID 1.
What can be the problem?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-09-30 08:42 AM
The NetBotz 750 A-link communication is built up as the picture shows.
The NetBotz 750 has two A-link connection when the first time I have started the systems I have connected one by one the sensor pods. The sensor pods received the ID numbers. POD 1- POD 6
I have started to connect the A-link cable to the secund A-link port on the NetBotz 750. The POD is getting the ID 1 another ID 88 and then ID 88.
The NetBotz 750 shows error message which was attached in my previous post.
This way can handle the NetBotz 750 the A-link cable and the sensor pods?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-10-01 01:38 AM
Hi Gabor,
Have you tried using 24v power supplies on every 4th sensor pod as you might have overloaded the A Link Bus ?? This has solved promblems like this for me before.
Try connecting them to only 1 port on the 750 and see if this works as you can cascade up to 12 sensor pod 150's
Regards,
Mike
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-10-01 09:53 AM
Hi Mike,
I have started with the pod number 1 and then followed by pod 2 end so on. I extend with 24v power supply every 3th sensor pod, which I connect after I have connected the A-link cable.
Everything was working well. When I have connected the pod 6 this pod has got the ID number 1. I have tried to work with the second A-link line which was started from the other A-link port from the NetBotz 750. In this line the first pod was getting the ID 1. In this point this was the third pod with ID number 1. If you look my previously attached picture the pod 1 ID has pod 1, pod 6, pod 7. Pod 8-10 is getting the 88 ID number.
The Netbotz 750 shows alarm (see my starting post)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-10-05 12:23 PM
I have reset the device and configured the IP parameters. The NetBotz has still alarms. I have updated the firmware, now it runs on 5.2.3 version.
It doesn’t recognize the sensor pod. I have deleted them before the reset.
Question, when I have deleted a sensor pod than can the NetBotz 750 recognize them again?
What can be the problem with this NetBotz 750 system?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-10-06 12:26 AM
Hi Gabor,
It might be no harm to log a ticket with your local support team, this might require some bus level debugging.
- Gavan
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-04-08 09:36 AM
Hello @GaborNovak ,
I did the exact same procedure as you did on my netbotz rack monitor 550, and now my internal pod has no readings (temperature, humidity and dew point).
Did you ever get this problem solved?
Can you please share how should I proceed?
Thanks in advance!
Best regards
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-04-09 07:06 AM
@Anonymous user
I had this issue with NetBotz 750 system.
Which NetBotz system are you using?
NetBotz 750 or NetBotz 550?
If you are using other NetBotz device it is recommend to start a new topic with the question. In that way we don’t mix the topic.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.