Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Schneider Electric Community
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
  • About GaborNovak
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
GaborNovak
GaborNovak
Contributor
‎2026-06-10
38
Posts
5
Likes Received
2
Likes Given
1
Solution

Community Badges

Open Hailing Frequencies - L3
Resistance is Futile - L3
Live Long and Prosper - L2
Open Hailing Frequencies - L2
+7
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
GaborNovak
GaborNovak

DCE add NetBotz 250 sensor to sub folder in map view

I would like to add a dry contact sensor to the map. The NetBotz 250A device is in the sub level 1 folder. I would like to add specific dry contact se...
EcoStruxure IT icon_circle EcoStruxure IT Forum
599 1 1

2025-03-21 12:22 AM

GaborNovak
GaborNovak

NetBotz 250 EOL/EOS

Does Schneider have EOL/EOS for NetBotz 250 system?
EcoStruxure IT icon_circle EcoStruxure IT Forum
1429 0 1

2022-12-16 08:34 AM

GaborNovak
GaborNovak

Data Center Expert supports old NetBotz 550 and NetBotz 200

The newest DCE 7.9.x support old NetBotz 550 and NetBotz 200 system?
EcoStruxure IT icon_circle EcoStruxure IT Forum
1350 0 1

2022-11-16 12:32 AM

GaborNovak
GaborNovak

NetBotz 570 emails through DCE server

With older DCE VM version it was possible to send emails through DCE server via NetBotz 570.The older DCE version was 7.6. The DCE private lan port wa...
EcoStruxure IT icon_circle EcoStruxure IT Forum
1662 1 2

2022-10-26 07:41 AM

GaborNovak
GaborNovak

NetBotz 250 wireless temperature sensor graph

I have installed a NetBotz 250 with 3 temp sensor. I can see the temperature reading. But there is no graph. I have added this NetBotz 250 device to t...
EcoStruxure IT icon_circle EcoStruxure IT Forum
2117 0 4

2022-09-21 05:25 AM

GaborNovak
GaborNovak

AP9631 web card host state meaning

Web card sending the following notification.Host State: DOWNHost State: UP What does it mean regarding to the UPS?Was this earlier the warm start stat...
EcoStruxure IT icon_circle EcoStruxure IT Forum
1568 1 1

2022-07-27 03:53 AM

GaborNovak
GaborNovak

NetBotz 250 minimum voltage threshold violation

NetBotz 250 keeps dropping the following errors. This NetBotz 250 is used to monitor the genset dry contacts. The environment temperature is not above...
EcoStruxure IT icon_circle EcoStruxure IT Forum
1375 0 1

2022-07-25 03:43 AM

GaborNovak
GaborNovak

PME DCE integration

DCE can connect to ION (PME) power monitoring expert.Does anyone have experience with PME integration to DCE?DCE can handle PME alarms? If the integr...
EcoStruxure IT icon_circle EcoStruxure IT Forum
2468 0 3

2022-02-01 02:43 AM

GaborNovak
GaborNovak

DCE backup notification if it’s failed

It is possible to get notification or active alarm when the backup fails? (In the server log I can See If there is some problem.)
EcoStruxure IT icon_circle EcoStruxure IT Forum
1015 0 0

2021-08-26 08:47 AM

GaborNovak
GaborNovak

DCE connected devices IP change

If I change a few device IP address, it is possible to use this new IP address without to lose the sensor data which was collected.
EcoStruxure IT icon_circle EcoStruxure IT Forum
2564 0 3

2021-07-02 01:18 AM

GaborNovak
GaborNovak

DCE home page scatter plot display

A customer has two NetBotz 570 which are connected to the DCE server. The webserver home screen is set up to show the two NetBotz temperature sensors....
EcoStruxure IT icon_circle EcoStruxure IT Forum
1794 0 2

2021-01-19 06:15 AM

Activity Feed
  • Got a Like for DCE add NetBotz 250 sensor to sub folder in map view. ‎2025-03-23 10:22 PM
  • Posted DCE add NetBotz 250 sensor to sub folder in map view on EcoStruxure IT Forum. ‎2025-03-21 12:22 AM
  • Got a Like for AP9631 web card host state meaning. ‎2024-05-05 11:44 PM
  • Posted NetBotz 250 EOL/EOS on EcoStruxure IT Forum. ‎2022-12-16 08:34 AM
  • Liked Re: Data Center Expert supports old NetBotz 550 and NetBotz 200 for spezialist. ‎2022-11-16 05:13 AM
  • Posted Data Center Expert supports old NetBotz 550 and NetBotz 200 on EcoStruxure IT Forum. ‎2022-11-16 12:32 AM
  • Posted Re: NetBotz 570 emails through DCE server on EcoStruxure IT Forum. ‎2022-11-04 04:23 AM
  • Got a Like for NetBotz 570 emails through DCE server. ‎2022-10-26 09:39 PM
  • Posted NetBotz 570 emails through DCE server on EcoStruxure IT Forum. ‎2022-10-26 07:41 AM
  • Posted NetBotz 250 wireless temperature sensor graph on EcoStruxure IT Forum. ‎2022-09-21 05:25 AM
  • Posted AP9631 web card host state meaning on EcoStruxure IT Forum. ‎2022-07-27 03:53 AM
  • Posted NetBotz 250 minimum voltage threshold violation on EcoStruxure IT Forum. ‎2022-07-25 03:43 AM
  • Posted PME DCE integration on EcoStruxure IT Forum. ‎2022-02-01 02:43 AM
  • Got a Like for Re: Rittal rPDU (CMC III Processing Unit) Association Issue. ‎2021-11-04 02:22 AM
  • Posted Re: Rittal rPDU (CMC III Processing Unit) Association Issue on EcoStruxure IT Forum. ‎2021-10-13 10:45 AM
  • Posted DCE backup notification if it’s failed on EcoStruxure IT Forum. ‎2021-08-26 08:47 AM
  • Posted DCE connected devices IP change on EcoStruxure IT Forum. ‎2021-07-02 01:18 AM
  • Posted Re: NetBotz POD device ID 88 on EcoStruxure IT Forum. ‎2021-04-09 07:06 AM
  • Posted DCE home page scatter plot display on EcoStruxure IT Forum. ‎2021-01-19 06:15 AM
  • Posted Re: Data Center Expert custom notification return to normal events on EcoStruxure IT Forum. ‎2021-01-11 11:44 PM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.