Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Toshiba G9000 UPS with EMD

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • Toshiba G9000 UPS with EMD
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Anonymous user
Not applicable

Posted: ‎2021-04-06 09:28 PM

0 Likes
3
2359
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
Posted: ‎2021-04-06 09:28 PM

Toshiba G9000 UPS with EMD

Hello all

I have a DDF created by APC for the G9000 v1 Remote Eye 4 card. It reads fine but does not read/pickup the EMD (environmental device) attached to it. I have looked though the MIBs provided by Toshiba and the MIB for the UPS does not have any OIDs for the EMD. But they do have a MID with readings for the EMD but that MIB has nothing for readings from the UPS such as input and output voltage and the like.

 

My question is "Is it possible to join these two MIBs together into one, and get a a DDF from that? or add the OIDs from the one that has them to the DDF for the G9000?

 

Really I only need 3 of the OIDs added they are as follows.

 

.1.3.6.1.4.1.186.1.19.2.5.254.5.1.0 - "The name assign to specific EMD." 

.1.3.6.1.4.1.186.1.19.2.5.254.5.2.0 - "The EMD temperature." 

.1.3.6.1.4.1.186.1.19.2.5.254.5.9.0 - "The EMD Humidity." 

Labels
  • Labels:
  • Data Center Expert
  • DDF
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 3
tjlaw
tjlaw Mentor
Mentor

Posted: ‎2021-04-08 06:57 AM

1 Like
2
2342
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
Posted: ‎2021-04-08 06:57 AM

Hi 

 

A quick solution is to use the supplemental OIDS function as follows: 

 

 

image.png

 

image.png

 

You can choose the sensor type from the drop-down menu. 

 

Or you can submit a DDF request for the corresponding DDF. 

 

BR, 

 

TJ

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

APC_Steve
APC_Steve Leader
Leader

Posted: ‎2021-04-08 07:05 AM

In response to tjlaw
1 Like
1
2340
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
Posted: ‎2021-04-08 07:05 AM

Just an FYI, supplemental OIDs do not work with text based values so the name won't work.

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

Anonymous user
Not applicable

Posted: ‎2021-04-10 06:20 AM . Last Modified: ‎2021-04-10 06:22 AM

In response to APC_Steve
1 Like
0
2325
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
Posted: ‎2021-04-10 06:20 AM . Last Modified: ‎2021-04-10 06:22 AM

Thank you I did not know that we could add supplemental OIDs. But sadly that did not work as the readings are without decimal like the reading for temperature is 600 in the OID but the real value is 60.0. Also they do not offer Fahrenheit as a reading on Celsius. But at least the humidity percentage I could add. It looks like the only way is to edit the current DDF to include these values.

 

In truth I was unsure if they could combine MIBs as the readings came from two MIBs for the same device (I really do not understand that one. But now they are charging for DDF creation for 3rd party devices. Of which I have asked why I am paying for support on nodes but it is not covered in that. 

 

Anyways Thank you for your help.

  • Tags:
  • english
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.