Ask our Experts
Didn't find what you are looking for? Ask our experts!
Schneider Electric support forum about installation, configuration, integration and troubleshooting of EcoStruxure Geo SCADA Expert (ClearSCADA, ViewX, WebX).
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-02-14 09:16 AM . Last Modified: 2023-05-02 11:48 PM
Hello all,
"localhost:8080 says
Application load failed: Unspecified error"
From the VirtualViewXAuthentication.log file:
2023-02-21 07:51:37: LogOn( [IN] userName = 'test_acct' )
2023-02-21 07:51:37: Sending request - requestCode = 500
2023-02-21 07:51:37: LogOn( [OUT] )
2023-02-21 07:51:37: Dispose( [IN] disposing = True )
2023-02-21 07:51:37: Disposing ScxComClient
2023-02-21 07:51:37: Disconnecting link in ScxComClient
2023-02-21 07:51:37: [PL3414:CL1] Virtual link disconnecting
2023-02-21 07:51:37: [PL3414] Changed to state 'Disconnected'
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-02-14 12:32 PM
You'll have to contact sales and request trial licenses.
You need the Database Server licensed and the Virtual ViewX server licensed.
Then from the HMI machine you will be able to access the Virtual ViewX using a HTML5 browser.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-02-14 02:06 PM
Hi Geoffpatton,
I have received trial licenses for both the Database Server and the Virtual ViewX server and have both up. My issue is setting up the VVX <-> VX comms now. It may be a profile issue, but I just wish there were a walk through that explained the process better than what I have found.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-02-14 02:24 PM
As far as I can remember once Virtual ViewX server is licensed it just works with the local ViewX.
The only problem I think I have had is that I installed the Virtual ViewX Server on a separate machine than the Database server and did not realize that I had to license the local ViewX Client as well. The Virtual ViewX server virtualizes multiple instances of the ViewX that is local to the machine it is installed on. The local ViewX has to be licensed and the Configure Connections app setup to connect to the server just like on the database server, other than that maybe set to local host and you need the machine name or ip address of the server on a remote client. If Virtual ViewX server is installed on the same machine as the database server it uses the ViewX that is licensed with the database server.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-02-14 02:59 PM
Setting up web servers and Virtual ViewX in particular has been getting more difficult with the increased complexities of security and infrastructure. SE have produced new resources to help customers:
Virtual ViewX Troubleshooting Guide
https://community.se.com/t5/Geo-SCADA-Knowledge-Base/Virtual-ViewX-Setup/ba-p/278269
Scripting Setup Guide (Updated)
Setup of ARR Reverse Proxy
https://community.se.com/t5/Geo-SCADA-Knowledge-Base/WebX/ba-p/279109?attachment-id=32978
I hope these are of help. If you have any feedback please post.
Thanks
Steve
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-02-20 08:24 AM
Hey Steve,
I appreciate you taking the time to answer my question (your videos as well). I'll go through these resources that you've provided and see where it takes me.
I'll keep the forum updated.
Thanks
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.