Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

3rd Party Devices with EcoStruxure Energy Hub and EcoStruxure Panel Server

EcoStruxure Energy Hub

This forum is dedicated to supporting EcoStruxure Energy Hub service providers and partners with system implementation, reporting skills growth, and in demonstrating profitable improvements in monitored sites. Ask questions, get expert answers and the latest offer news, provide feedback and share community experience and knowledge!
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
  • EcoStruxure Power & Grid
  • EcoStruxure Energy Hub
  • 3rd Party Devices with EcoStruxure Energy Hub and EcoStruxure Panel Server
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Thierry_Baudard
Commander Thierry_Baudard Commander
8
EduardoFainblum
Commander EduardoFainblum Commander
6
Mathew_Losey
Lt. Commander Mathew_Losey Lt. Commander
5
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to EcoStruxure Energy Hub
Start a Topic
Mathew_Losey
Lt. Commander Mathew_Losey Lt. Commander
Lt. Commander

Posted: ‎2023-12-15 10:32 AM . Last Modified: ‎2023-12-15 10:42 AM

6 Likes
0
10674
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
Posted: ‎2023-12-15 10:32 AM . Last Modified: ‎2023-12-15 10:42 AM

3rd Party Devices with EcoStruxure Energy Hub and EcoStruxure Panel Server

This is a knowledge base post to share a summary on integrating third party, non-Schneider Electric energy, water or gas meters with EcoStruxure Energy Hub using custom models for EcoStruxure Panel Server.

 

To integrate 3rd party devices with Energy Hub, a custom model for the Panel Server gateway is needed.  To create and export custom models for Panel Server, EcoStruxure Power Commission - Web tool is available.

 

Access the EcoStruxure Power Commission Web (EPC-W) tool here.

 

Mathew_Losey_0-1702664806598.png

 

Creating a 3rd party Custom Model for Panel Server 

Follow the existing EPC-Web Documentation on creating a custom Model/Driver with changes to the following steps below. 

 

New Panel Server Energy Model/Driver Product creation 

Energy Hub uses the Product type to assign it an Energy Hub Concept type.  When you create a Product Type please make sure the following steps are done. 

  • Brand: Cannot be left as default “Schneider Electric” 
  • Product Family: Select the family type matching to the Concept type you want from Appendix A. 
  • Product Range: can be anything 
  • Product: can be anything 
  • Commercial Reference: Must be left blank 

Mathew_Losey_1-1702664853186.png

 

 New Panel Server Water or Gas Model/Driver Product Creation 

When creating a Model/Driver for a Water or Gas meter you need to have more specific values entered into the New Product Fields.   When you create a Product Type please make sure the following steps are done. 

  • Brand: <Cannot be left as default “Schneider Electric”> 
  • Product Family: I/O Device 
  • Product Range: Standard_Pulse 
  • Product: <can be anything> 
  • Commercial Reference: GENERIC_PULSE_INPUT 

Mathew_Losey_2-1702664853187.png

 

 After the model/driver has been imported into the Panel server and the device has been added using the 3rd party driver then the last step is to set the device’s commodity in the Panel Server to match WATER or GAS depending on what the device is recording. 

Mathew_Losey_3-1702664853188.png

 

 Creating Panel Server model/driver for a PLC 

To implement this work around the Client/Slave device you are trying to communicate to must be able to handle multiple different UnitIDs communicating with it.  In addition, it must allow multiple connections to the device. 

 

Currently you cannot build a single driver that splits up into multiple devices in Energy Hub.  This means that if you build a Single PLC driver to import 10 water meters, Energy Hub currently cannot break that PLC into 10 different water meter devices. 

 

The work around is to build a separate driver for each device you want to split off from your PLC.  For Example, a PLC that has readings from 5 different water meters would have 5 drivers.  One for each water meter you wanted to import into Energy Hub. 

Each separate driver would point to different registers on the PLC.  (The register mapped to the measurement you want to read for the separated device). 

 

When you are adding devices to the Panel server, you would select each of the separate drivers and the connect it to the PLC using the same IP Address but a different UnitID. 

 

NOTE: Some ModbusTCP devices do not allow separate different UnitIDs to be connected to them.  Please check the Device/PLC Documentation to make sure it can handle multiple separate unitIDs. If this is the case you might have to switch to using a SiteServer to handle communicating with those devices as SiteServer allows the setup of the same UnitIDs to talk to a single device. 

 

Map the specific EEH Measurements to the Model/driver that is created. 

Energy Hub uses select Measurements in Energy Hub.  Refer to Appendix B and Appendix C to see what measurements you need to map and the Name (HMIName-Long) you need to use in the EPC-Webpage Measurement Name Lookup. 

 

FAQ

Q: Does Energy Hub support 3rd party devices? 

A: Yes, Energy Hub now officially supports 3rd party devices using a custom model for EcoStruxure Panel Server. 

 

Q: What types of 3rd party devices are supported? 

A: As a first step, we will support 3rd party power, energy, water and gas meters.  We will only support devices that provide measurements that Energy Hub can view in the standard dashboards with currently available subscriptions.  

 

Q: How do we create custom models for Panel Server? 

A: Custom models for EcoStruxure Panel Server can be created by approved users of EcoStruxure Power Commission Web (EPC-W).  

 

Q: Are there any limitations I should be aware of? 
A: The same general limitations that exist today with EcoStruxure Panel Server apply to 3rd party devices.  For example, multi-circuit meters, data concentrators (e.g. one device with an IP Address but multiple Modbus IDs), are not supported.  The Panel Server alarms/events publishing limit also applies in the same way for 3rd party devices as for standard devices – see the cloud gateway load calculator.   

 

Q: Can we get alarms and events from 3rd party devices with a Panel Server Custom Model? 

A: No, like other software offers, we are not able to retrieve 3rd party device alarms / events through a standard modbus register table.  Energy Hub can generate software threshold alarms based on measurement data we retrieve from the devices. 

Mathew Losey
EcoStruxure Energy Hub Global Offer Manager
Attachments
Labels
  • Labels:
  • Knowledge Base
  • Tips and Tricks
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.