Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Send New InviteClose
Announcements
Find the latest Product Announcesments on The Exchange here: PA-00941 - EcoStruxure Building Advisor - New Features Q2 2023
In EBO 2024 (6.0), when install or upgrade the Advanced Minimum Polling Interval will be changed from default (0) to the following. However, for sites that have not upgraded or are using Multi-version systems, there should be recommendations to change if less than the new default values. If the values remain at the previous default of 0, the EBO Servers will attempt to poll at the default 500ms, which can overwhelm the communications trunk.