Subscribing is a smart move!
You can subscribe to this forum after you log in or create your free account.
Have ideas on how we can improve the EcoStruxure Building Advisor? Please share and get votes from our Community to influence development efforts.
Subject | Author | Likes | Views | Latest Post | Replies | |
---|---|---|---|---|---|---|
Feature:
1) In BMS Health report generation wizard, add an option checkbox to include a device-li...
| 0 | 594 | 2 | |||
Feature: Change the axis for the controller memory and CPU usage graphs to display the actual dat...
| 0 | 639 | 3 | |||
Could we get a graph showing forced point count against time I.E. to (hopefully) show a reduction o...
| 0 | 935 | 4 | |||
Can we have an associated username visible for the forced points table?
| 0 | 551 | 2 | |||
Hi,
Would it be possible to have a view whereby the customer site list is removed from the le...
| 1 | 857 | 3 | |||
Hi,
Is it possible to add programmable Xenta to the BMS Health? So that they are included in t...
| 0 | 511 | 2 | |||
Hi,
On the Asset Health Report, under "Automated Analysis Checks", I have found if there is ...
| 0 | 690 | 3 | |||
The summary of categories devices on page 4 in the reports are very useful.
If this could be more...
| 0 | 951 | 5 | |||
If there are no avoidable costs identified on a healthy site then the user should be able to desele...
| 0 | 571 | 3 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.