What card readers and technology can be used with Continuum Access Control Systems

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • What card readers and technology can be used with Continuum Access Control Systems
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • Product_Support
    Product_Support
  • Cody_Failinger
    Cody_Failinger
  • sesa119747
    sesa119747
  • Dave_Shore
    Dave_Shore
  • CraigEl
    CraigEl

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2535 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

What card readers and technology can be used with Continuum Access Control Systems

Picard Product_Support
‎2018-09-11 09:28 AM

Last Updated: Administrator CraigEl Administrator ‎2022-08-08 09:52 PM

Issue

What card readers and technology can be used with Continuum Access Control Systems

Product Line

Andover Continuum

Environment

Continuum

Cause

Need to know what card readers will work with Continuum Access Control Systems

Resolution

The card reader and card technology is not relevant to the Continuum Controller, as this is used between the card (tag, fob or other) and the reader. This allows the use of the standard technologies available today, including fingerprint and other biometric based access as well as cards, fobs and tags.

The signal that comes from the reader must be serial data input type Wiegand or ABA (or Clock & Data)

USB, Ethernet, RS485, RS232 inputs are not accepted.

  • NOTES
  • The exact input type and maximum data bits can only be determined by checking the hardware, firmware and Continuum version combination being used.
  • Retina, fingerprint, facial recognition and other biometric based systems that are connected to Continuum Access Controllers will store the biometric information and still be connected via the serial data Wiegand or ABA to the Continuum Controller.
  • The current Continuum access controllers also accept an 8 bit burst for PIN numbers from keypads
  • See Where can I find datasheets, install guides and other information on HID Electronic Access Control p...
  • ABA (or Clock & Data) this was often used with Magnetic Swipe technology which has mostly been phased out
  • Standard Wiegand Formats within Continuum
    • Infinity 37-Bit
    • AC 4+4 32-Bit
    • Wiegand 26-Bit
    • CK 34-Bit
    • G 32-Bit
    • HIDCorp1000 35-Bit - Some restrictions
    • Custom
Labels (1)
Labels:
  • Andover Continuum
Tags (1)
  • Find more articles tagged with:
  • 11762
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.