Issue
Supported Import and Export File Formats in Graphics Editor
Product Line
EcoStruxure Building Operation
Environment
- TGML
Cause
Clarification of Supported File Formats in TGML
Resolution
TGML Overview
TGML (TAC Graphics Markup Language) is an XML-based declarative language designed for creating dynamic 2D graphics within EcoStruxure Building Operation. Graphics developed in the Graphics Editor are saved with the .TGML
file extension.
When a graphic is created, a TGML root object is automatically generated and placed at the bottom of the Objects tree in the editor’s object pane. This root object also serves as the default layer in the Graphics Editor workspace and cannot be deleted.
For more info: TGML File Format