Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

PCT Error: "VBoxManager.exe: error: Nonexistent host networking interface", "Failed to open project."

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • PCT Error: "VBoxManager.exe: error: Nonexistent host networking interface", "Failed to open project."
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • SharlinaRe
    SharlinaRe
  • RandyDavis
    RandyDavis
  • CraigEl
    CraigEl
  • chris_clerc
    chris_clerc
  • Jonathan
    Jonathan
  • Taylor_Leach
    Taylor_Leach
  • StephenYang
    StephenYang
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
6761 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

PCT Error: "VBoxManager.exe: error: Nonexistent host networking interface", "Failed to open project."

Picard Product_Support
‎2018-09-10 09:30 AM

Last Updated: Administrator CraigEl Administrator ‎2023-09-12 12:13 AM

Issue

During certain situations, it may be required to switch from a hardwired to a wireless connection or wireless to a hardwired. In addition, you may be required to replace a failed NIC card with a new variant that may or may not be the same in terms of connection type. Other more rare situations where a technician travels with a laptop that has PCT "SERVER" mode installed would also be affected.

Example:

PCT Version - 1.1.2.57 Server mode was set up on a physical server that has two NIC cards. The initial setup was performed on NIC1 and now we are required to utilize NIC 2 which is wireless as a temporary solution.

NIC card 1 is disabled and NIC card 2 is set up with the same IP details as NIC card1. In addition, the wireless network is an extension of the original network that was configured in NIC card 1. The server then gets rebooted.

Once the server is up you start PCT and attempt to open a project.

1-Try to open a project.PNG

You receive the following errors:

"VBoxManager.exe: error: Nonexistent host networking interface"
"Failed to open project." 
2- Project fails to open.PNG
3- Vm fails to start.PNG

 

Product Line

EcoStruxure Building Operation

Environment

  • Windows Client versions (64 Bit Only)

  • Windows Server versions (64 Bit Only)

  • PCT SERVER versions (64 Bit OS Only )

  • SBO Project Configuration Tool All versions

Cause

During the initial setup of Project Configuration Server mode, you are prompted to select a network interface card from a list of available NICs. PCT requires that you continue to use the same interface and if you change your connection type at the windows level PCT has no method of knowing this and will not be able to connect to previously created projects.

PCT will produce the following complaint as seen in the log below:

"Nonexistent host networking interface"

4- PCT Log with Adapter Error.PNG

 

You can find the log path as follows:

C:\ProgramData\Schneider Electric StruxureWare\Building Operation\Project Configuration Tool\loggermodule

"ProjectsModule.log"

5- PCT Error LOG Windows Folder Location.PNG

 

Resolution

There are two solutions to address this:

  1. Revert your connection type back to the original Network Interface Card. Reboot the machine. Open PCT and attempt to get back into the project.6- Project Opens when Original Nic is restored.PNG
  2. If the idea is to stick with a different NIC, you would simply need to reinstall PCT and select the new NIC during "SERVER" mode setup. Reboot the machine. Open PCT and attempt to get back into the project.
Labels (2)
Labels:
  • EcoStruxure Building Operation
  • Project Configuration Tool
Tags (7)
  • Find more articles tagged with:
  • 19760
  • command
  • oracle
  • RandyDavis22
  • run
  • SharlinaRenwall22
  • unable
Was this article helpful? Yes No
34% helpful (1/3)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.