Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Installing PCC-10 or PCLTA-21 network cards on a Windows 7 PC

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Installing PCC-10 or PCLTA-21 network cards on a Windows 7 PC
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • CraigEl
    CraigEl
  • PeterLarsen
    PeterLarsen
  • sesa115370
    sesa115370
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
4049 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Installing PCC-10 or PCLTA-21 network cards on a Windows 7 PC

Picard Product_Support
‎2018-09-10 06:17 AM

Last Updated: Administrator CraigEl Administrator ‎2022-08-08 06:00 PM

Issue

Procedure for installing PCC-10 or PCLTA20/21 network cards on a Windows 7 PC

Product Line

TAC Vista

Environment

  • Vista
  • Menta
  • LonMaker
  • Windows 7

Cause

Installation procedure differs from earlier versions of driver software.

Resolution

The PCC-10 and PCLTA-20/21 network cards work on Windows 7 (32 bit) PCs when the OpenLDV 4.0 driver is installed. This driver is installed automatically when Lonmaker Turbo SR4 is installed, but if this version of Lonmaker is not present the driver must be installed manually.  The latest drivers can be obtained from the Echelon download site: http://www.echelon.com/support/downloads

Note: The PCLTA-20/21 card is only supported on 32bit windows operating systems. For 64bit systems use a NIC-USB as mentioned in this article: Computer will not recognize NIC709-USB.

Install the drivers before fitting the card in the PC.

Please note that OpenLDV4.0 requires .NET Framework 3.5 SP1.  This is not included as a subset of .NET Framework 4 or later, so must be installed separately.  You can have multiple versions of .NET framework installed on the same PC.

The following description is for the PCLTA-21 but the PCC-10 is similar.

To change the system image or perform diagnostics, you must go to Control Panel and open the Lonworks Interfaces application:

  1. Click Start on the taskbar, point to Settings, click Control Panel, and then open the LONWORKS Interfaces application.
  2. Click the PCLTA-21 interface in the list view on the left side of the user interface to display the interface's properties in the details pane in the right side.
  3. The details pane lists the PCLTA-21 card's system image and transceiver properties.
  4. To change the system image used by the PCLTA-21 card, click anywhere in the NI Application
    property, click the box to the right, and then browse to and select the desired system image from
    the LonWorks\Images\PCLTA21 folder.

Note: For more information on configuring, testing, and diagnosing the PCLTA-21 network interface, see the LonWorks Interfaces online help.

Labels (1)
Labels:
  • TAC Vista
Tags (1)
  • Find more articles tagged with:
  • 7221
Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.