Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Echelon Node Utility with Loytec NIC-USB Network Interface

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Echelon Node Utility with Loytec NIC-USB Network Interface
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • CraigEl
    CraigEl
  • RyanSuar
    RyanSuar
  • RobertAndriolo
    RobertAndriolo
  • Benji
    Benji
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
3343 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Echelon Node Utility with Loytec NIC-USB Network Interface

Picard Product_Support
‎2018-09-11 03:23 PM

Last Updated: Administrator CraigEl Administrator ‎2022-08-08 08:56 PM

Issue

Echelon Node Utility with Loytec NIC-USB Network Interface

Product Line

EcoStruxure Building Operation, Satchwell MicroNet, Satchwell Sigma, TAC IA Series, TAC Vista

Environment

  • Microsoft Windows 7 32-bit
  • Echelon Node Utility 2.04
  • Echelon OpenLDV 4.0
  • Loytec NIC-USB network interface
  • Loytec NIC driver version 4.1.3

Cause

There is a need to run Echelon Node Utility using Loytec network interfaces.

Resolution

The easiest way to accomplish this, is to use the NodeUtil Launcher. This program scans the registry for known interfaces. It was created by an active Community member.
* Do take note Schneider Electric Product Support does not provide support for the NodeUtil Launcher - for support please write the developer of the tool.

Below are two methods to manually achieve this if you don't want to use the tool.


Here are 2 methods to run Node Utility using Loytec NIC-USB network interface.
Method 1 involves accessing the Windows registry to check the path name of the Loytec network interface. We are not modifying any entries in the registry but as always, we should be careful when we access the Windows registry. Using Windows registry incorrectly can cause serious problems that may require you to reinstall Windows.
Method 2 will configure the Loytec NIC-USB to use LON1. If you have used an Echelon LonWorks interface as LON1, you will need to detach it before you can use this method.


Method 1

  1. Run Loytec LConfig tool.
  2. With the Loytec NIC-USB network interface connected, go to the 'USB' tab and test the connectivity
  3. Run Windows registry editor (Start > Run > regedit).
  4. Navigate to the path HKEY_LOCAL_MACHINE\SOFTWARE\LonWorks\DeviceDrivers. The interfaces will be shown here. Look for the interface with '_LDV'.
  5. Run Windows Command Prompt and navigate to the Node Utility software directory (whichever directory you have put Node Utility) and run NodeUtil using the command nodeutil -D"". See example below.


Method 2

  1. Run Loytec LConfig tool.
  2. With the Loytec NIC-USB network interface connected, go to the 'USB' tab and test the connectivity.
  3. Click on the 'Advanced' button. Check the option 'LON1 Support for device' and select the appropriate device in the drop down list. You will need to reboot the computer for this to take effect.
  4. Once the computer has restarted, run Windows Command Prompt and navigate to the Node Utility software directory (whichever directory you have put Node Utility) and run NodeUtil. Node Utility should now run.

Labels (5)
Labels:
  • EcoStruxure Building Operation
  • Satchwell BAS & Sigma
  • Satchwell MicroNet
  • TAC IA Series
  • TAC Vista
Tags (1)
  • Find more articles tagged with:
  • 15021
Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.