Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

EBO 2.0 does not support the SBO SmartX Display Tech Tool

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • EBO 2.0 does not support the SBO SmartX Display Tech Tool
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • DavidChild
    DavidChild
  • HenrikTarpgaard
    HenrikTarpgaard
  • CraigEl
    CraigEl
  • David_Kendrick
    David_Kendrick
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2591 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

EBO 2.0 does not support the SBO SmartX Display Tech Tool

Picard Product_Support
‎2018-09-10 09:11 AM

Last Updated: Administrator CraigEl Administrator ‎2022-08-11 02:04 AM

Issue

Moving from SBO 1.9 to EBO 2.0 and above does not allow the Tech Tool to be used on SmartX Displays.

Product Line

EcoStruxure Building Operation

Environment

EBO 2.0

Cause

The SmartX Display Tech Tool is being discontinued in EBO 2.0 in favour of a completely overhauled Webstation which is now designed for use on Tablets and Smart Phones as well as PCs.

Resolution

Tablet used here is the T580

First of all, the tablet itself will need to be brought up to Android OS 7 minimum (OS 8 works as well). Depending on how long it has been since the tablet was last connected online, the Android OS may require a number of updates before it reaches Android OS 7.

Most importantly, when finished the tablet must have a firmware number ending with T580XXU2BQL1 or above.  (E.g. T580XXU2BQI9 is lower than T580XXU2BQL1). If for some reason this is not the case then please manually update the software instead.

1 Build Number.png

Next contact the Schneider Electric Global Expert Support Team, to obtain the latest versions of SmartX Kiosk and AD-Link application. One visible change in the Kiosk is that it now includes a Chrome shortcut as standard. The AD-Link is still required to establish the connection between the Tablet and the SmartX Server over USB using IP address 192.168.42.116. It is only the Tech Tool itself, that is discontinued.

Once the AD-Link has been opened and connected, Chrome can then be used to connect to the SmartX Server using the same 192.168.42.116 Address. Successful logon can then be achieved using the same Username and Password as the Tech Tool.

2 Web Log In.png

The new and improved Webstation interface can be accessed that is optimised for Tablet and Smart Phone screens

3 Web Look.png

In some cases, the customer may not want Chrome's open browser interface and may instead wish to lock down the appearance of the browser to be closer to that of the older Tech Tool. If this is the case, please refer to 'Locking Down' Chrome and Webstation in EBO 2.0 for SmartX Displays.

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (2)
  • Find more articles tagged with:
  • 19915
  • HenrikTarpgaard19
Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.