Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Default Device ID / Device Instance of SE7000 series BACnet controllers

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Default Device ID / Device Instance of SE7000 series BACnet controllers
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • RobertAndriolo
    RobertAndriolo
  • CraigEl
    CraigEl
  • sesa194431
    sesa194431
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2732 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Default Device ID / Device Instance of SE7000 series BACnet controllers

Picard Product_Support
‎2018-09-10 11:33 PM

Last Updated: Administrator CraigEl Administrator ‎2022-08-08 11:48 PM

Issue

Without knowing the Device ID / Device Instance these devices cannot add to the MSTP network in the AS or ES.

Product Line

Andover Continuum, EcoStruxure Building Expert, EcoStruxure Building Operation, Field Devices

Environment

  • Automation Server
  • Enterprise Server
  • BACnet
  • SE7000

Cause

Only the MAC ID / Com Address is shown in the display but not the Device ID / Device Instance.

Resolution

SE7200x Models

Default Device ID is set to: 72000 + MAC

  • Where MAC is the current MAC address of the device.

The device ID will also be upgraded as soon as there is a change to the device’s MAC.

For example, when a SE7200F5045B controller with a MAC address of 41 is connected to a network, its default Device Name will be SE7200F5x45B-41 and its default Device ID will be 72041.

SE73xxx Models

Default Device ID is set to: 73000 + MAC

  • Where MAC is the current MAC address of the device.

The device ID will also be upgraded as soon as there is a change to the device’s MAC.

For example, when a SE7300C5045B controller with a MAC address of 63 is connected to a network, its default Device Name will be SE7300C5x45B-63 and its default Device ID will be 73063.

Click here for the Integration Manual.

Please refer to the SE7300 series BACnet controller does not come online in StruxureWare Building Operation if SE7300 controller does not come online.

Labels (4)
Labels:
  • Andover Continuum
  • EcoStruxure Building Expert
  • EcoStruxure Building Operation
  • Field Devices
Tags (2)
  • Find more articles tagged with:
  • 12516
  • se73000
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.