Configuring Custom 37-Bit as well as Infinity 37-Bit Card Format

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Configuring Custom 37-Bit as well as Infinity 37-Bit Card Format
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • Product_Support
    Product_Support
  • Roger_Bently
    Roger_Bently
  • DavidChild
    DavidChild
  • CraigEl
    CraigEl

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
5506 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Configuring Custom 37-Bit as well as Infinity 37-Bit Card Format

Picard Product_Support
‎2018-09-10 10:51 AM

Last Updated: Administrator CraigEl Administrator ‎2021-11-30 01:12 PM

Issue

How to configure Custom 37-Bit as well as Infinity 37-Bit Card Format

Product Line

Access Expert

Environment

  • Access Expert
  • Server 2012 and Above
  • Version 2
  • Version 3
  • Hosted 
  • Premise

Cause

When configuring Custom 37-Bit as well as Infinity 37-Bit Card Formats, the settings are different based on the Facility Code, Card Length and Card Formats. The HEX code generated in Live Monitoring can be deciphered to get the correct set of values required to make this work for your application. If you are unable to do so, please contact PSS and open a ticket so that they can help.

Resolution

The following settings on the screen shots show how to configure Custom, HID Formats and Infinity 37-Bit Formats, please pay attention to the one that will work for your specific application:

    1. Open and log on to the respective Access Expert Instance
    2. Select the tab Access Configuration to create a new Card Format
      Creating a new format1.jpg
    3. Name the format accordingly in the description field, this can be used for Infinity 37-Bit if so desired
      Creating NF1.jpg
    4. Add the card range by clicking on the page Icon on the Number Range
    5. There is a Standard, HID Managed 37-Bit (not Infinity 37) in the drop down in the Card Format Presets
      Infinity 37 Custom.jpg
      Infinity 37 FC and Standard.jpg
    6. This can be used by default but if you have a Custom 37-Bit Format and the Facility Code is known, however the Start Bit and Length will be different.
      Infinity 37 Format.jpg
    7. An Infinity 3 Bit Format will use the Parity Bits
      Infinity 37 Bit.jpg
    8. Create the new format per the screen shots and configure accordingly.
    9. Once complete, click on Save or Save and Close, reboot the controller.
Labels (1)
Labels:
  • EcoStruxure Access Expert
Tags (3)
  • Find more articles tagged with:
  • 19223
  • CraigEllis21
  • DavidKendrick21
Was this article helpful? Yes No
100% helpful (1/1)

Link copied. Please paste this link to share this article on your social media post.

You’ve reached the end of your document

WHAT’S NEXT?

Ask our Experts

Didn't find what you are looking for? Ask our experts!

My Dashboard

Check out the new Feeds and activities that are relevant to you.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.