Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

BACnet bCX MSTP network loses communication when a b-Link is added or removed

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • BACnet bCX MSTP network loses communication when a b-Link is added or removed
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Cody_Failinger
    Cody_Failinger
  • CraigEl
    CraigEl
  • DavidFisher
    DavidFisher
  • PaulFr
    PaulFr
  • Alan_Wood
    Alan_Wood
  • Dave_Shore
    Dave_Shore
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2825 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

BACnet bCX MSTP network loses communication when a b-Link is added or removed

Product_Support
‎2018-09-11 05:54 AM

Last Updated: CraigEl Champion ‎2022-08-08 11:19 PM

Issue

BACnet bCX MSTP network loses communication when a b-Link is added or removed

Product Line

Andover Continuum

Environment

MSTP b3 bCX4040  b-Link

Cause

The bCX MSTP circuitry is slightly different to the b-Link  MSTP circuitry , thus under some circumstances, other faults on the MSTP network can cause communication to change, when the network is connected via a b-Link

Resolution

  1. If an MSTP network is installed correctly, then it will operate correctly at all speeds up to 76.8k (assuming all devices operated up to this speed)
  2. If the MSTP network is not stable up to 76.8k, or adding or removing a b-Link causing a loss of communication, then it is likely there is some fault on the network.
    (adding or removing the end of line termination resistors, is also a useful fault finding option)
  3. The bCX MSTP components are slightly different to the b-Link MSTP components, thus under some circumstances, other faults on the MSTP network can cause communication to be lost, when the network is connected via a b-Link

Example
This has been seen when third party variable speed drives (VSDs) were connected to a bCX MSTP network (these unit had switchable termination resistors that by default were in circuit)
The communication was ok at a low speed (19200) connected directly to a bCX, but when the network was put on the secondary side of a b-Link, the communication failed.

Once the termination resistors were switched out of circuit, the communication via the b-Link was fine.

In the example above the VSDs were by ABB

Related: How to change the Baud Rate of a field bus (Infinet or Bacnet MSTP) when there is an Infilink or B-l...

Labels (1)
Labels:
  • Andover Continuum
Tags (2)
  • Find more articles tagged with:
  • 13759
  • blink
Was this article helpful? Yes No
100% helpful (3/3)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.