Issue
Older sites still have ACX781 controllers installed, but the cabinet keys are missing. Users want to know if replacement keys can be ordered.
Product Line
Andover Continuum
Environment
ACX781 Cabinet Enclosure
Cause
The ACX781 controller was discontinued in 2007, and the stock of cabinet lock/key assemblies has been depleted.
Resolution
- Replacement cabinet keys for ACX781 controllers are no longer available.
- If access is required, consider replacing the cabinet lock with a standard lock assembly from a local hardware supplier.
- For long-term support, plan to upgrade to current-generation controllers.