Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

http command using cmd file

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • http command using cmd file
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
BillP Leader
2150
Teken
Teken
144
Techie_apc
Techie_apc
83
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
Solved Go to Solution
Back to APC UPS for Home and Office Forum
Start a Topic
Solved
Lokoto
Lokoto
Explorer

Posted: ‎2025-05-13 08:02 AM

0 Likes
2
1042
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
Posted: ‎2025-05-13 08:02 AM

http command using cmd file

I have network devices that are powered with Back-UPS ES 650G2. The UPS supports my internal network. I would like commands to be executed via http when power is restored. e.g. "http://10.10.10.32/relay/off". How do I set the command in the cmd file of the UPS so that on a "No longer on battery" event I get that command or a series of commands executed.

Labels
  • Labels:
  • Home & Office - UPS & Software
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
fredkm
fredkm Troubleshooter
Troubleshooter

Posted: ‎2025-05-15 07:52 AM

1 Like
1
1011
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
Posted: ‎2025-05-15 07:52 AM

The UPS can't execute command files. You could use PowerChute Serial Shutdown software for this purpose. On the Event Configuration page you can configure execution of a command file if the 'No Longer on Battery' event occurs. I guess that in command file you could use 'curl' to execute your http command(s).

 

Keep in mind that PowerChute Serial Shutdown will safely shutdown the connected server (based on options configured in Shutdown Settings page). If your server is down PowerChute Serial Shutdown of course will not detect that power is restored. And the command file will not be executed. You could enable 'wake on AC' in your BIOS so your server will automatically boot up again when power is restored. This will also start PowerChute Serial Shutdown service. In the Event Configuration page you probably want to enable the same command file for the 'Monitoring Started' event. This event occurs after PowerChute Serial Shutdown has started up an starts monitoring the UPS.

 

Hope this helps. Further Questions just ask.

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 2
fredkm
fredkm Troubleshooter
Troubleshooter

Posted: ‎2025-05-15 07:52 AM

1 Like
1
1012
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
Posted: ‎2025-05-15 07:52 AM

The UPS can't execute command files. You could use PowerChute Serial Shutdown software for this purpose. On the Event Configuration page you can configure execution of a command file if the 'No Longer on Battery' event occurs. I guess that in command file you could use 'curl' to execute your http command(s).

 

Keep in mind that PowerChute Serial Shutdown will safely shutdown the connected server (based on options configured in Shutdown Settings page). If your server is down PowerChute Serial Shutdown of course will not detect that power is restored. And the command file will not be executed. You could enable 'wake on AC' in your BIOS so your server will automatically boot up again when power is restored. This will also start PowerChute Serial Shutdown service. In the Event Configuration page you probably want to enable the same command file for the 'Monitoring Started' event. This event occurs after PowerChute Serial Shutdown has started up an starts monitoring the UPS.

 

Hope this helps. Further Questions just ask.

Reply

Link copied. Please paste this link to share this article on your social media post.

Lokoto
Lokoto
Explorer

Posted: ‎2025-05-16 11:47 PM

In response to fredkm
0 Likes
0
983
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
Posted: ‎2025-05-16 11:47 PM

Thank you @fredkm ! That was exactly that I needed! Made it and tested it. Works great.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.