Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84576members
353847posts

UPS for UTS10BI

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
1Diesel_apc
Cadet
0 Likes
2
136

UPS for UTS10BI

This was originally posted on APC forums on 1/21/2013


I recently set up a UTS10BI and am using an old UPS 1250ns (750 watts). I am looking for something that can handle the 1800 watt max of the transfer switch.
The problem I see is most UPS's of this size require a 20- 30 amp power source. The convenience outlet is sub rated to 12A from 15 per electrical code.
If I use another outlet from a 20A circuit I may be able to get closer to required charging current.

Thanks for your time


Accepted Solutions
Boatingrtb_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
136

Re: UPS for UTS10BI

This was originally posted on APC forums on 3/21/2013


I purchased a xantrax inverter & use a dual 12v battery bank.

works great

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
136

Re: UPS for UTS10BI

This reply was originally posted by Angela on APC forums on 2/4/2013


i think the largest VA UPSs we have that are 12A rated, 15AMP total are 1500VA - something like a BR1500G or SMT1500. those probably are around 850 watts though only.

Boatingrtb_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
137

Re: UPS for UTS10BI

This was originally posted on APC forums on 3/21/2013


I purchased a xantrax inverter & use a dual 12v battery bank.

works great