Smart-UPS 1000 shutting down PC during scheduled Self-Test
APC UPS for Home and Office Forum
Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2021-06-2905:32 AM. Last Modified: 2024-03-2111:05 PM
Smart-UPS 1000 shutting down PC during scheduled Self-Test
Hello UPS Experts,
I am using a Smart-UPS 1000 for a private single PC since March 2010, and for some months it performed flawlessly. However, since 6 weeks the PC is being forced into Hibernation Mode every 2 Weeks, and upon closer inspection I could see that those shutdowns coincide with the pre-set "14 Days Self Test" of the Smart-UPS 1000. No power loss occured at all, and the PC can be "woken up" again without data loss, so it seems like a controlled shutdown. Windows gives the infomation that "The Battery was low" on reboot, just like on a Laptop...
The PC is running Windows 7 64 bit, connection via USB, Smart-UPS 1000 firmware revision is 652.19.I, the UPS load is just 20% and the battery is always up at 100%.
For the moment I simply disabled the automatic Self Test (set to "Never"), but I would like to know if this an expected behaviour, or a bug in the Smart-UPS 1000 or in the Middleware / driver / Host application?