Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

RS 1000 battery backup doesn't last long in Windows

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • RS 1000 battery backup doesn't last long in Windows
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
Administrator BillP Administrator
2151
Teken
Kirk Teken
123
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
Solved Go to Solution
Back to APC UPS for Home and Office Forum
Start a Topic
Solved
Anonymous user
Not applicable

Posted: ‎2021-07-11 10:59 PM . Last Modified: ‎2024-03-19 11:41 PM

0 Likes
1
1812
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
Posted: ‎2021-07-11 10:59 PM . Last Modified: ‎2024-03-19 11:41 PM

RS 1000 battery backup doesn't last long in Windows

I have a wierd problem. My APC unit is quite old and model is RS 1000 (BR-1000IN). It has two battries inside connected in series. After the batteries are fully charged 100% as per windows battery indicator, I restart the PC in BIOS and let it run. It works for 30 minutes or so.

However, the same fully charged batteries, when PC is run in windows, it doesn't work for even 10 minutes. Battery percentage dips very fast and then windows shutsdown gracefully (configured to shutdown at 20% in windows power options). Any idea what the problem is?

I was using APC PowerChute software and it was showing load of ~120W. Assumed, may be the software is causing issue, I uninstalled it and started using Windows native power option, but the problem remains.

I have already tried recalibration, disconnected, re-connected batteries etc, nothing seems to help. These two set of batteries were working great for like 45 minutes when it was newly installed a year ago.

Is load the problem? but then why the same configuration PC worked earlier on these batteries.

Any suggestion help would be appreciated.

Labels
  • Labels:
  • Back-UPS & Surge Protectors
  • Tags:
  • 1000
  • backup
  • bios
  • but
  • in
  • problem
  • rs
  • windows
  • works
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
BillP
Administrator BillP Administrator
Administrator

Posted: ‎2021-07-11 10:59 PM . Last Modified: ‎2024-03-19 11:40 PM

0 Likes
0
1812
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
Posted: ‎2021-07-11 10:59 PM . Last Modified: ‎2024-03-19 11:40 PM

Hi,

When the system is running the BIOS it is consuming less power since it is using fewer resources. When running Windows the system will consume more power to provide the needed resources.

If recalibrating the batteries did not resolve the issue you can either replace the batteries or as you mentioned the "unit is quite old” replace the UPS.

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
BillP
Administrator BillP Administrator
Administrator

Posted: ‎2021-07-11 10:59 PM . Last Modified: ‎2024-03-19 11:40 PM

0 Likes
0
1813
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
Posted: ‎2021-07-11 10:59 PM . Last Modified: ‎2024-03-19 11:40 PM

Hi,

When the system is running the BIOS it is consuming less power since it is using fewer resources. When running Windows the system will consume more power to provide the needed resources.

If recalibrating the batteries did not resolve the issue you can either replace the batteries or as you mentioned the "unit is quite old” replace the UPS.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.