Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84849members
354308posts

RS 1000 battery backup doesn't last long in Windows

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
kdagli_apc
Crewman
Crewman
0 Likes
1
282

RS 1000 battery backup doesn't last long in Windows

This was originally posted on APC forums on 8/30/2015


I have a wierd problem. My APC unit is quite old and model is RS 1000 (BR-1000IN). It has two battries inside connected in series. After the batteries are fully charged 100% as per windows battery indicator, I restart the PC in BIOS and let it run. It works for 30 minutes or so.

However, the same fully charged batteries, when PC is run in windows, it doesn't work for even 10 minutes. Battery percentage dips very fast and then windows shutsdown gracefully (configured to shutdown at 20% in windows power options). Any idea what the problem is?

I was using APC PowerChute software and it was showing load of ~120W. Assumed, may be the software is causing issue, I uninstalled it and started using Windows native power option, but the problem remains.

I have already tried recalibration, disconnected, re-connected batteries etc, nothing seems to help. These two set of batteries were working great for like 45 minutes when it was newly installed a year ago.

Is load the problem? but then why the same configuration PC worked earlier on these batteries.

Any suggestion help would be appreciated.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
282

Re: RS 1000 battery backup doesn't last long in Windows

This reply was originally posted by Bill on APC forums on 8/31/2015


Hi,

When the system is running the BIOS it is consuming less power since it is using fewer resources. When running Windows the system will consume more power to provide the needed resources.

If recalibrating the batteries did not resolve the issue you can either replace the batteries or as you mentioned the "unit is quite old” replace the UPS.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
283

Re: RS 1000 battery backup doesn't last long in Windows

This reply was originally posted by Bill on APC forums on 8/31/2015


Hi,

When the system is running the BIOS it is consuming less power since it is using fewer resources. When running Windows the system will consume more power to provide the needed resources.

If recalibrating the batteries did not resolve the issue you can either replace the batteries or as you mentioned the "unit is quite old” replace the UPS.