Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84862members
354344posts

ES-550 Just Will Not Stop Beeping 4 Times/30 Seconds

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
whitedavidp_apc
Crewman
Crewman
0 Likes
3
2151

ES-550 Just Will Not Stop Beeping 4 Times/30 Seconds

This was originally posted on APC forums on 8/24/2015


I have a couple of these UPS units. One of them keeps beeping 4 times/30 seconds (with light off during beeps) even when AC power has been restored. What does this mean? I know this is the signal for battery operation. But it should stop, right? I have powered the unit off/on and still it does this. Driving me crazy.

Thanks!


Accepted Solutions
whitedavidp_apc
Crewman
Crewman
0 Likes
0
2151

Re: ES-550 Just Will Not Stop Beeping 4 Times/30 Seconds

This was originally posted on APC forums on 8/24/2015


I do not use the surge-only outlets. But I plugged in a phone charger and found no power in those outlets. I just realized that this unit has a circuit breaker on the rear. Normally, I don't think I have enough load on it to cause an overload. But sure enough, I checked and found the breaker needed to be pressed. So the unit was still running on battery to support the load I have there and it seems like it would not switch back to AC power until the breaker was reset.

So FYI to others out there.

See Answer In Context

BillP
Administrator Administrator
Administrator
0 Likes
0
2151

Re: ES-550 Just Will Not Stop Beeping 4 Times/30 Seconds

This reply was originally posted by Jordan on APC forums on 8/25/2015


David,

As you have found, the 4 beeps every 30 seconds does indicate on battery and checking the surge only outlets was a great way to test that.  If the circuit breaker on the unit is tripped, the unit will operate on battery to provide power to battery backup outlets only.

Regards,

See Answer In Context

Elfnet_apc
Crewman
Crewman
0 Likes
0
2151

Re: ES-550 Just Will Not Stop Beeping 4 Times/30 Seconds

This was originally posted on APC forums on 2/5/2016


Ok what if the breaker is NOT tripped and the unit is still beeping 4 times every 30 seconds? 

See Answer In Context

3 Replies 3
whitedavidp_apc
Crewman
Crewman
0 Likes
0
2152

Re: ES-550 Just Will Not Stop Beeping 4 Times/30 Seconds

This was originally posted on APC forums on 8/24/2015


I do not use the surge-only outlets. But I plugged in a phone charger and found no power in those outlets. I just realized that this unit has a circuit breaker on the rear. Normally, I don't think I have enough load on it to cause an overload. But sure enough, I checked and found the breaker needed to be pressed. So the unit was still running on battery to support the load I have there and it seems like it would not switch back to AC power until the breaker was reset.

So FYI to others out there.

BillP
Administrator Administrator
Administrator
0 Likes
0
2152

Re: ES-550 Just Will Not Stop Beeping 4 Times/30 Seconds

This reply was originally posted by Jordan on APC forums on 8/25/2015


David,

As you have found, the 4 beeps every 30 seconds does indicate on battery and checking the surge only outlets was a great way to test that.  If the circuit breaker on the unit is tripped, the unit will operate on battery to provide power to battery backup outlets only.

Regards,

Elfnet_apc
Crewman
Crewman
0 Likes
0
2152

Re: ES-550 Just Will Not Stop Beeping 4 Times/30 Seconds

This was originally posted on APC forums on 2/5/2016


Ok what if the breaker is NOT tripped and the unit is still beeping 4 times every 30 seconds?