Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84567members
353835posts

ES 350 beeping 4 times every 30 second, but green light still on

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
WendyLouWho_apc
Cadet
0 Likes
3
637

ES 350 beeping 4 times every 30 second, but green light still on

This was originally posted on APC forums on 3/26/2010


After moving to a new house, I plugged my ES 350 in, and the green light is on. But it beeps 4 times every 30 seconds. The knowledge base talks about this beeping with an amber light, but mine is green.

Is it working, or not? How do I stop the beeping.

Wendy
wendyluwhu@aol.com

Tags (1)

Accepted Solutions
shasuren_apc
Lieutenant
Lieutenant
0 Likes
0
639

Re: ES 350 beeping 4 times every 30 second, but green light still on

This was originally posted on APC forums on 4/12/2010


Wendy, There are two types of the Beeps on this UPS. There are "Notification Beeps" and "Warning Beeps" . You can silence only the "Notification Beeps" through Power Chute Software. But there is no option to silence the "Warning Beeps".

To resolve the issue, please perform cold start and check.

1. Unplug all connected devices from the unit including the interface cable if connected.
2. Switch the unit off if it is on
3. Unplug the unit from the wall outlet.
4. Then press the power switch and release it as soon as you hear a long beep. Please Note: We need to release the button before the long beep ends.
5. The unit should come up on battery and beep 4 times every 30 seconds
6. Then plug in the UPS to wall outlet, the Green LED will glow.

See Answer In Context

BillP
Administrator Administrator
Administrator
0 Likes
0
638

Re: ES 350 beeping 4 times every 30 second, but green light still on

This reply was originally posted by Laurie on APC forums on 4/12/2010


There's no reason to cold start this UPS.

The kbase is talking about different models. The BE models don't have an amber light, they have a green one that usually flashes periodically when on battery, just like Judy asked. That's normal for on battery operation.

However, I'm not sure why it's on battery. You could try the UPS in a different outlet, confirm there is working power there. You can also change the sensitivity via the PowerChute software - there may be noise on the line that is causing the unit to operate on battery.

See Answer In Context

juangele_apc
Lt. Commander
Lt. Commander
0 Likes
0
639

Re: ES 350 beeping 4 times every 30 second, but green light still on

This was originally posted on APC forums on 3/29/2010


Hi Wendy,

May I know the exact model number of the unit? Is the green light flashing while it's beeping?

See Answer In Context

3 Replies 3
shasuren_apc
Lieutenant
Lieutenant
0 Likes
0
640

Re: ES 350 beeping 4 times every 30 second, but green light still on

This was originally posted on APC forums on 4/12/2010


Wendy, There are two types of the Beeps on this UPS. There are "Notification Beeps" and "Warning Beeps" . You can silence only the "Notification Beeps" through Power Chute Software. But there is no option to silence the "Warning Beeps".

To resolve the issue, please perform cold start and check.

1. Unplug all connected devices from the unit including the interface cable if connected.
2. Switch the unit off if it is on
3. Unplug the unit from the wall outlet.
4. Then press the power switch and release it as soon as you hear a long beep. Please Note: We need to release the button before the long beep ends.
5. The unit should come up on battery and beep 4 times every 30 seconds
6. Then plug in the UPS to wall outlet, the Green LED will glow.

BillP
Administrator Administrator
Administrator
0 Likes
0
639

Re: ES 350 beeping 4 times every 30 second, but green light still on

This reply was originally posted by Laurie on APC forums on 4/12/2010


There's no reason to cold start this UPS.

The kbase is talking about different models. The BE models don't have an amber light, they have a green one that usually flashes periodically when on battery, just like Judy asked. That's normal for on battery operation.

However, I'm not sure why it's on battery. You could try the UPS in a different outlet, confirm there is working power there. You can also change the sensitivity via the PowerChute software - there may be noise on the line that is causing the unit to operate on battery.

juangele_apc
Lt. Commander
Lt. Commander
0 Likes
0
640

Re: ES 350 beeping 4 times every 30 second, but green light still on

This was originally posted on APC forums on 3/29/2010


Hi Wendy,

May I know the exact model number of the unit? Is the green light flashing while it's beeping?