Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

BX2200MI and Linux apcupsd repeated battery detach/battery attach events

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • BX2200MI and Linux apcupsd repeated battery detach/battery attach events
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
BillP Leader
2150
Teken
Teken
147
voidstar_apc
voidstar_apc
83
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
Back to APC UPS for Home and Office Forum
Start a Topic
syntesys
syntesys
Explorer

Posted: ‎2024-07-18 02:13 AM . Last Modified: ‎2024-07-18 02:15 AM

0 Likes
3
1539
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
Posted: ‎2024-07-18 02:13 AM . Last Modified: ‎2024-07-18 02:15 AM

BX2200MI and Linux apcupsd repeated battery detach/battery attach events

 

Hello all,

I'm using a BX2200MI, and I keep getting the following messages from apcupsd:

Jun 14 08:23:11 envy apcupsd[1682]: Battery disconnected.
Jun 14 08:23:12 envy apcupsd[1682]: Battery reattached.
Jun 14 08:23:13 envy apcupsd[1682]: Battery disconnected.
Jun 14 08:23:14 envy apcupsd[1682]: Battery reattached.
Jun 14 08:25:04 envy apcupsd[1682]: Battery disconnected.
Jun 14 08:25:05 envy apcupsd[1682]: Battery reattached.
Jun 14 08:30:07 envy apcupsd[1682]: Battery disconnected.
Jun 14 08:30:08 envy apcupsd[1682]: Battery reattached.
Jun 14 08:31:51 envy apcupsd[1682]: Battery disconnected.
Jun 14 08:31:52 envy apcupsd[1682]: Battery reattached.

 

I'm using apcupsd in debian 12.

Labels
  • Labels:
  • Home & Office - UPS & Software
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 3
Teken
Teken
Champion

Posted: ‎2024-07-19 09:02 AM

0 Likes
2
1502
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
Posted: ‎2024-07-19 09:02 AM

How does the system behave when using APC PCPE / PCSS software?!? This simple test will either affirm the unit and USB cable is performing correctly. ☝️

 

If the problem is NOT seen using the official APC (PCPE / PCSS) software it’s -APCUPSD.

 

If the APC PCPE / PCSS software behaves the same way. Move the USB cable to another port and if that corrects the problem there was a bad port.

 

If the problem remains change out the USB cable while ensuring the new cable is indeed a (Data & Power) cable! 

If the problem goes away it was a bad cable. If the problem continues verify the USB port on the UPS is physically fine. If so then the USB port on the UPS may be defective. 


You may consider using NUT instead to see if the problem goes away due to improper drivers / configuration / support. 

Lastly, it goes without saying if the power management is set to energy saving better check it’s not the OS putting the USB port or anything else into sleep / turned off state.

 

Other considerations is if the cable is too long vs the factory cable. You can resolve this by using a powered USB HUB or active USB cable. 

Reply

Link copied. Please paste this link to share this article on your social media post.

syntesys
syntesys
Explorer

Posted: ‎2024-07-20 08:34 AM

In response to Teken
0 Likes
1
1467
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
Posted: ‎2024-07-20 08:34 AM

Already did all the tests before writing here. We bought 5 BX2200MI UPSes, and connected to the system with the cable we found in the box. With Windows (during configuring PowerChute and testing alle the 5 machines) never had the problem, so, it seems that the problem is the libusb driver used by apcupsd. I found this post in your forum, but cannot compile because the command "./configure enable-usb with-generic-usb" gives me an error that the flag "enable-usb" does not exists.

Reply

Link copied. Please paste this link to share this article on your social media post.

Teken
Teken
Champion

Posted: ‎2024-07-23 06:55 AM

In response to syntesys
0 Likes
0
1466
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
Posted: ‎2024-07-23 06:55 AM

You may consider using NUT instead. 👍
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.