Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
A update of PostgreSQL prevents EcoStruxure IT Gateway version 1.23 and newer from being installed on CentOS 7 or RHEL 7.
Attempts to update an existing Gateway to version 1.23 will fail.
For existing Gateway installations, deploy a new Gateway 1.23 on a supported Linux operating system. To retain sensor history, follow these instructions:
After you download and install the Gateway, go to the default address https://<server name or IP address>and set the password for the system administrator. The default username isadmin.
Configure device credentials.
Create device credential settings for discovery and polling SNMPv1, SNMPv3, NetBotz, and Redfish devices. You can reuse these credentials for all your device discoveries and add additional credentials as needed.
Create file transfer settings for device configuration, firmware update, and other EcoStruxure IT features to function properly.
Discover devices
Enter an IP address or IP address range, or import an IP address list to easily discover devices.