Gateway default ports

System requirements

System requirements for EcoStruxure IT Gateway software including operating system, CPU and RAM, disk space, firewall, and supported browsers
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
  • EcoStruxure IT Help Center
  • EcoStruxure IT Help Center Categories
  • Gateway
  • System requirements
  • Gateway default ports
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • EcoStruxure IT Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

EcoStruxure IT Support

Submit a support request for additional assistance with EcoStruxure IT software.

Request Support
Back to System requirements
Start a Topic
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
1 Like
17317 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Gateway default ports

Picard EcoStruxureIT
‎2019-02-15 05:29 AM

If your firewall blocks the Gateway default ports listed here, or any non-default ports you specified, you must add firewall exceptions for these ports.

The information in this article pertains to the latest version of EcoStruxure IT Gateway.

Web server

Communication between the Gateway and your web browser on the intranet uses the following port:

Name Port Direction Type Description
Web server 443 INBOUND TCP Web browser access to Gateway interface

You can specify the ports used by the Gateway web server when you install the Gateway software.

 

Device communication

Communication between the Gateway and your devices on the intranet uses the following ports:

Name Port Direction Type Description
FTP 21 OUTBOUND TCP Transfer device configurations, firmware binaries, and logs
SCP 22 OUTBOUND TCP Transfer device configurations, firmware binaries, and logs
SNMP 161 OUTBOUND UDP SNMP device polling and discovery
  1062 INBOUND UDP

SNMP traps

  162 INBOUND UDP

SNMP traps (default for most third party devices)

  8011 INBOUND TCP HTTP Service log capture (available on select devices)
NetBotz HTTPS 443 OUTBOUND TCP HTTPS NetBotz device polling and discovery
  8453 INBOUND TCP HTTPS NetBotz traps
NetBotz HTTP 80 OUTBOUND TCP HTTP NetBotz device polling and discovery
  8010 INBOUND TCP HTTP NetBotz traps
Modbus TCP 502 OUTBOUND TCP Modbus TCP device polling and discovery
Redfish 443 OUTBOUND TCP Redfish server polling and discovery

See Configure SNMP trap ports


EcoStruxure IT communication

Communication between the Gateway and EcoStruxure IT over the internet uses the following port.

Name Port Direction Type Description
EcoStruxure IT 443 OUTBOUND TCP EcoStruxure IT Gateway communication with EcoStruxure IT cloud.

 

Local system only

Firewalls do NOT need to open external access to these ports. This information is provided to help avoid port conflicts. 

Name Port Direction Type Description
Database port 5432 INBOUND TCP Local System ONLY - Used by the Gateway software to communicate with its database.

Note: The database port is subject to change on software update. A free port is automatically selected for the database during the update process.

 

Gateway appliance specific

Gateway appliance version 1.10 and newer

Name Port Direction Type Description
Gateway 22 INBOUND TCP Gateway application command line interface access
Gateway 2222 INBOUND TCP

For support use only 

Gateway appliance OS command line interface access via SSH

Note: You must first access the Gateway CLI from the appliance private network on port 22 to enable the SSHD service, and then follow the instructions provided by support.

See Gateway appliance command line interface (CLI) - version 1.10 and newer

See EcoStruxure IT Gateway appliance installation and setup - version 1.10 and newer for more information.

 

Gateway appliance version 1.9 and older

Communication between the Gateway appliance's Webmin interface and your web browser.
Note: Webmin is only accessible from the private network of the Gateway appliance.

Name Port Direction Type Description
Webmin 10000 INBOUND TCP Web browser access to the Gateway appliance's Webmin setup and configuration interface.

See EcoStruxure IT Gateway appliance installation - version 1.9.0 and older for more information.

More information

In addition to the firewall of your host system, your IT department might have firewalls and proxies in place that could prevent Gateway from communicating with EcoStruxure IT or your devices. 

Contact your IT department if they are running firewalls that are blocking required ports.

If your organization uses a proxy, see the instructions in these articles for configuring the Gateway:

System requirements for EcoStruxure IT Gateway
Installing and setting up EcoStruxure IT Gateway

Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.