SpaceLogic KNX Forum
Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
Link copied. Please paste this link to share this article on your social media post.
Hello!
I'm using the Valve Drive Controller to Control basic and additional heating.
I figured out that I have an issue with the Cycle time for automatic transimission parameter.
Every time I set the setpoint high enouht to power on the additional stage - It works until the Cycle time for automatic transmission passes. Then the Additional stage receives a '1' and a "0" right after. After that the additional stage remains switched off. Basic stage working perfectrly fine.
Now I've switched off the Cycle time for automatic transimission and the system is running well, but I know that I'm messing up with something.
Please let me know if you have any suggestions!
Thank you so much!
Link copied. Please paste this link to share this article on your social media post.
Hi KisevcompanyLTD!
Sorry for the late reply! Can you provide more details (Telegram log) in order to see clearly what happens and what are the dedicated temperatures.
Link copied. Please paste this link to share this article on your social media post.
Hello, and thank you for your answer!
Can you please tell me where can I send some Screenshots - Because the forum doesn't allow me to Attach any.
Thank you so much!
Link copied. Please paste this link to share this article on your social media post.
Hi KisevcompanyLTD!
To "Can you please tell me where can I send some Screenshots - Because the forum doesn't allow me to Attach any. "
Hmm ... this sounds strange!
There are two ways to attach pictures:
1. You include them directly into your text at the right position. To do so you can use the camera icon to include your picture. Of course your picture needs to be in accepted format.
2. You can use the dedicated functionality to attach file to your thread.
Again, of course your picture needs to be in accepted format.
Maybe you can try with a different browser?
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.