Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84865members
354358posts

Isagraf *.pia file restore to *.hie

Remote Operations Forum

Collaborate and share knowledge on the extensive range of remote systems and devices, including SCADA radios and RTUs, on the Schneider Electric Exchange Remote Operations (formerly SCADA & Telemetry) forum. From commissioning SCADA integration devices and software, to enhancing existing installations or troubleshooting, connect with a global community of experts and users. Subscribe today.

HDP
Ensign
Ensign
0 Likes
2
421

Isagraf *.pia file restore to *.hie

Hello,

 

I have .pia file and would like to restore it to get a .hie file.

 

I have a demo version of the Isagraf installed but it does not support restore from archived project.

 

Is there any other way to restore the .pia file? (eg. unzip)

 

Is there a way to get a trail version of Isagraf 3.55  that is fully functional?

 

Thanks in ad

2 Replies 2
Joel_Weder
Commander Commander
Commander

Re: Isagraf *.pia file restore to *.hie

Hello Hardik Patel,

 

You are correct that a demo version of the software cannot be used to restore the original .pia file. Our Tech Support team can assist you with this, however, if you send them the file and explain your issue. Here are two ways you can reach them:

 

Support for Australia, New Zealand, Pacific regions:

techsupport.pz@se.com

13 73 28 (13 SEAU)  inside Australia

0800 652 999 in side New Zealand

 

Alternately, support for Americas, Middle East and Asia is:

1-888-226-6876  or...

SupportTRSS@se.com

 

Joel Weder
Remote Operations Specialist
Schneider Electric
HDP
Ensign
Ensign
0 Likes
0
391

ThanksRe: Isagraf *.pia file restore to *.hie

Thank you Joel, I will contact them.