Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PowerLogic T300 - Getting SOE event time and convertin it to Modbus register

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • PowerLogic T300 - Getting SOE event time and convertin it to Modbus register
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Araceli_Monje Mentor
74
JuanRayo
JuanRayo Mentor
40
Arun-kumar_PS
Arun-kumar_PS Mentor
33
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Related Products
product field
Schneider Electric
PowerLogic T300

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
Anonymous user
Not applicable

Posted: ‎2020-12-22 12:21 AM . Last Modified: ‎2025-05-26 01:49 AM

0 Likes
2
1943
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
‎2020-12-22 12:21 AM

PowerLogic T300 - Getting SOE event time and convertin it to Modbus register

May I ask how to get T300 SC150 (CB OPEN/CLOSE, ES OPEN/CLOSE) SOE event TIME and convert to Modbus and assign it to a Modbus Register address?

 

As we need to mapping the CB / ES exact OPEN CLOSE TIME and put it on HMIGTO touch screen and this Touch Screen model only supply Modbus TCP.

 

 

Many thanks.

 

Tony Leung

  • Thumbnail of PowerLogic T300
    Schneider Electric
    PowerLogic T300
View products (1)
Labels
  • Labels:
  • Application cases
  • PowerLogic P3
  • PowerLogic T300
Tags (3)
  • Tags:
  • english
  • PowerLogic T300
  • SOE
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Anonymous user
Not applicable

Posted: ‎2021-01-13 07:28 PM . Last Modified: ‎2021-01-13 07:37 PM

0 Likes
0
1932
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
‎2021-01-13 07:28 PM

The only reason why the customer do not accept using the smartphone / tablet / embedded windows ..etc... is because those OS will release the latest update service pack OS update every months, and under the customer company policy, they must update it for the security reason, and they are not willing to spend the manpower to do  those update every months since there are 15,000+ substations, so they end up with the Schneider GTO series HMI touchscreen since the GTO do not have the OS update issue but it has very limited function.

 

Correct me if i am wrong that as far as i know Modbus is not a time based protocol that do not have the time stamping on every single TX RX message, only those time stamping data protocol would be supported (IEC104 / DNP3 / IEC61850 /  a proper SCADA on windows... etc).

 

And also the problem of T300 https web console do not have the ability to do the custom HMI design drawing, lets said my architecture has other devices such as protection relay , M580 PLC, ComX510, Power Meters.....and i cannot draw those on https web because there is no such function.

 

So here comes my question was    since I had already collected the real time stamp SOE time on the T300 https EVENT log page,     is there any way to get the value from the event log table and brings the string value to the Modbus as a bit word format to transmit the time log to the HMI through modbusTCP.....but it seems no one would do such custom works to get the value this way, but thanks Jean-Yves and appreciate for your reply.

See Answer In Context

Tags (1)
  • Tags:
  • english
Reply
Replies 2
JYPOC
JYPOC Mentor
Mentor

Posted: ‎2021-01-13 01:47 AM . Last Modified: ‎2021-01-13 01:48 AM

0 Likes
1
1936
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
‎2021-01-13 01:47 AM

Hi Tony,

 

The only way to reuse the time-stamping data coming from SC150 open/close control & status is to utilize a SCADA protocol that is fitted with time-stamping feature (and Modbus is not one of them: if you have a time-stamping capability then it is not a standard Modbus version but a proprietary one... and there are many of them with no compatibility between them).

 

If you really want to have a permanent HMI attached, the only solution to get the source time-stamping data would be to use a HMI model capable of accessing to T300 embedded webserver through HTTPS, or capable to operate with a standard time-stamped protocol.

 

Can you please describe a bit the architecture and the reason to have a HMI here? Why not use a Smartphone or a tablet to connect in HTTPS via Wifi to the T300 webserver? That would be way more secure than just using Modbus...

 

BR - Jean-Yves
  • Thumbnail of PowerLogic T300
    Schneider Electric
    PowerLogic T300
View products (1)
Tags (5)
  • Tags:
  • Distribution Automation
  • easergy t300
  • english
  • modbus
  • secondary substation
Reply
Anonymous user
Not applicable

Posted: ‎2021-01-13 07:28 PM . Last Modified: ‎2021-01-13 07:37 PM

0 Likes
0
1933
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
‎2021-01-13 07:28 PM

The only reason why the customer do not accept using the smartphone / tablet / embedded windows ..etc... is because those OS will release the latest update service pack OS update every months, and under the customer company policy, they must update it for the security reason, and they are not willing to spend the manpower to do  those update every months since there are 15,000+ substations, so they end up with the Schneider GTO series HMI touchscreen since the GTO do not have the OS update issue but it has very limited function.

 

Correct me if i am wrong that as far as i know Modbus is not a time based protocol that do not have the time stamping on every single TX RX message, only those time stamping data protocol would be supported (IEC104 / DNP3 / IEC61850 /  a proper SCADA on windows... etc).

 

And also the problem of T300 https web console do not have the ability to do the custom HMI design drawing, lets said my architecture has other devices such as protection relay , M580 PLC, ComX510, Power Meters.....and i cannot draw those on https web because there is no such function.

 

So here comes my question was    since I had already collected the real time stamp SOE time on the T300 https EVENT log page,     is there any way to get the value from the event log table and brings the string value to the Modbus as a bit word format to transmit the time log to the HMI through modbusTCP.....but it seems no one would do such custom works to get the value this way, but thanks Jean-Yves and appreciate for your reply.

Tags (1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.